cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U5A9J-DK1 USB Device as mass storage standalone via sdmm1 emmc

tod
Associate III

I want to use the EMMC as USB storage space, but I encountered another issue: I am trying to access the EMMC via SDMM1, and after implementing the MSC-related functions (read, write, USBD_STORAGE_GetMediaLastLba, USBD_STORAGE_GetMediaBlocklength) in ux_device_msc.c, the formatting operation on the PC side fails. The error message says: "Please insert a disk into the removable disk."
I have already verified that after initializing SDMM1, the EMMC can be accessed and read/write operations are successful.

What could be the reason for this issue?

The attached file is my project.

tod_0-1757730569995.png

ux_device_msc.c:

tod_2-1757730678625.png

tod_4-1757730856986.png

 

tod_3-1757730698364.png

 

 

 

10 REPLIES 10
tod
Associate III

Hi @FBL 

Thank you so much for your help! With your assistance, I have successfully formatted it as well.
However, I noticed that the file read/write transfer speed is very slow (1-2 MB/s). Is it possible to improve the read/write speed by adding ThreadX or using DMA?