2023-11-28 3:35 AM
Hello ST Community,
I'm facing a MIPI DSI configuration issue with my STM32U5A9 and TFT LCD. When using PHY DSI as the DSI lane byte clock source, my code fails with a timeout on HAL_DSI_ShortWrite. When I switch to PLL3P, the initialization proceeds, but the LCD displays distorted images.
Request for Assistance: I'm new to MIPI and suspect a misconfiguration in clock settings. Any insights on proper configurations or similar experiences with STM32U5A9 MIPI DSI would be greatly appreciated.
Details:
Thank you,
2023-12-01 9:21 AM
Characters have been successfully displayed on the LCD; however, they appear inverted and mirrored. Assistance in identifying the underlying issue would be greatly appreciated.
Your guidance in this matter would be highly appreciated.
2023-12-01 9:56 AM
First try
/**
* @brief Start test pattern generation
* @PAram hdsi pointer to a DSI_HandleTypeDef structure that contains
* the configuration information for the DSI.
* @PAram Mode Pattern generator mode
* This parameter can be one of the following values:
* 0 : Color bars (horizontal or vertical)
* 1 : BER pattern (vertical only)
* @PAram Orientation Pattern generator orientation
* This parameter can be one of the following values:
* 0 : Vertical color bars
* 1 : Horizontal color bars
* @retval HAL status
*/
HAL_StatusTypeDef HAL_DSI_PatternGeneratorStart(DSI_HandleTypeDef *hdsi, uint32_t Mode, uint32_t Orientation)after this work next step is framebuffer setup...
2023-12-05 1:14 AM - edited 2023-12-05 1:16 AM
Dumping the framebuffer and displaying it on GIMP confirms that the transmitted framebuffer is accurate, but there seems to be a misinterpretation by the Display controller.
I've attempted various configurations on the controller's side to address the issue, but the text continues to display as mirrored.
Alternating the MX bit in the this register, had not impact on the outcome - Any ideas would be much appreciated!
2023-12-12 9:51 AM
Hello,
@MM..1 @KDJEM.1 @Tesla DeLorean
I'm encountering challenges with the ST7796S display controller while attempting to implement certain commands. While some commands, like turning on the display or inverting colors, have the desired impact, the font appears inverted in the displayed image.
Upon inspecting with a scope, it appears that DSI is utilizing the HS clock, and despite my attempts, I haven't been successful in transitioning it to LP clock usage. This clock transition seems crucial during command transmission.
I have a few specific questions:
1. How can I configure the MIPI of U5 to transition from HS mode to LP mode?
2. What could be causing the controller to understand some commands while failing to comprehend others?
3. Are there specific measures I can take to address these issues effectively?
Any assistance or guidance on resolving these concerns would be greatly appreciated.
Thank you.
2025-09-20 2:48 AM - edited 2025-09-22 12:38 AM
Same Issue and after everything I didn't find any proper solution to this.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.