STM32U5A9 boot fail at low temperatures
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-23 8:42 AM
Hi,
We have a design that at normal temperatures runs fine (21C). If it goes below 0C it starts failing to boot.
The system has the Secure Boot Secure Firmware Update (SBSFU) system on it. We found that putting a delay at the start of the main() function in bl2_main.c seems to allow it to run. The delay needs to be about half a second.
Then as we reduce the temperature towards -40C we find we need to increase the delay to over a second to get it to work.
Does this sound familiar to anyone? Any ideas what could be going on?
Thanks
Nigel
Solved! Go to Solution.
- Labels:
-
STM32U5 series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-24 9:22 AM
Thanks all for the suggestions, we've found the problem.
It's related to the MCUBOOT_EXT_LOADER functionality. In boot_platform_init() towards the end there is a check for a BUTTON_PIN state and if high it tries to run a loader image. In our system this pin is not connected and must be floating high when cold causing it to attempt to run the loader image which also looks like it doesn't work.
It is not obvious to know this has to be configured and it is not helped that this pin is defined within the boot_hal.c file see https://github.com/STMicroelectronics/STM32CubeU5/blob/main/Projects/B-U585I-IOT02A/Applications/SBSFU/SBSFU_Boot/Src/boot_hal.c
To solve this we will probably disable MCUBOOT_EXT_LOADER as we probably don't need it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-23 9:48 AM
Do your crystals/oscillators have slow startup times?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-23 9:56 AM
Probably an external hardware issue; eg, clocks (as @Uwe Bonnes said), power supply, reset ...
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-23 12:53 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-24 12:34 AM
Hi,
Thanks all.
We don't believe it's external, we've checked reset against Vdd coming up and Vdd is stable before reset starts rising. The HSE is not active yet, the SBSFU uses the MSI clock. If I connect a debugger using STM32CubeProgrammer (v2.16.0) and use the 'Fault Analyzer' it indicates both instruction and data access faults (IACCVIOL, DACCVIOL).
Could some setup of the MSI in SBSFU need changing?
Thanks
Nigel
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-24 1:14 AM
Is external memory involved?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-24 1:44 AM
No, only using internal memory (FLASH and RAM)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-24 6:35 AM
Dear @NPato,
We need some information to share with experts:
- Can you check the status of RCC_CR_MSISRDY flag when it fails to boot (set or reset) ? Also, if you are using ST HAL check whether HAL_RCC_OscConfig returns HAL_TIMEOUT ?
- Are you using STM32U5A9J-DK board ?
Best Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-24 8:26 AM
> Are you using STM32U5A9J-DK board
No, this is our own HW design, which runs fine above 0C.
> Can you check the status of RCC_CR_MSISRDY flag when it fails to boot
When I connect the Stm32CubeProgrammer and use the registers page to look at RCC_CR it has value 0x0300F035, MSISON and MSISRDY bits are high.
> Also, if you are using ST HAL check whether HAL_RCC_OscConfig returns HAL_TIMEOUT ?
It's in the SBSFU code which I'm not overly familiar with. I'm not sure it's getting as far as running the SystemClock_Config() function. Has the ROM bootloader already brought up the MSI?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-24 8:30 AM
@NPato wrote:> Are you using STM32U5A9J-DK board
No, this is our own HW design
Does the DK run OK at the same temperature?
A complex system designed from scratch never works and cannot be patched up to make it work.