cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U58I-IOT02A : UART write is not printing on putty terminal

ram_jan
Associate II

Hi Team,

Currently I am using STM32U58I-IOT02A  Board and implementing UART Transmit and receive, I am seeing that it is not printing anything on the PUTTY terminal, Can anyone suggest me how to handle this issue. I have tried to send with HAL_UART_Transmit() and printf() commands both and it no outputs on the console.

 

code is pasted below :

 

static void MX_USART3_UART_Init(void)
{
/* USER CODE BEGIN USART3_Init 0 */
/* USER CODE END USART3_Init 0 */
/* USER CODE BEGIN USART3_Init 1 */
/* USER CODE END USART3_Init 1 */
huart3.Instance = USART3;
huart3.Init.BaudRate = 115200;
huart3.Init.WordLength = UART_WORDLENGTH_8B;
huart3.Init.StopBits = UART_STOPBITS_1;
huart3.Init.Parity = UART_PARITY_NONE;
huart3.Init.Mode = UART_MODE_TX_RX;
huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart3.Init.OverSampling = UART_OVERSAMPLING_16;
huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart3.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart3) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&huart3, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&huart3, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&huart3) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART3_Init 2 */
/* USER CODE END USART3_Init 2 */
}
HAL_GPIO_WritePin(uart_e_GPIO_Port, uart_e_Pin, SET); //ph13
HAL_GPIO_WritePin(ph15_GPIO_Port, ph15_Pin, SET); // ph15
RS232_Send(RS232_ACC, "USART3 Ready\r\n");
HAL_StatusTypeDef RS232_Send(RS232_Port port, const char *data)
{
HAL_StatusTypeDef status = HAL_OK;
snprintf((char *)tx_buffer[port], RS232_TX_BUFFER_SIZE, "%s", data);
status = HAL_UART_Transmit_IT(rs232_uart[port], tx_buffer[port], strlen((char *)tx_buffer[port]));
return status;
}

 

Edit: code formatting

4 REPLIES 4
Gyessine
ST Employee

hello @ram_jan 

You didn't use the correct USART. Based on the user manual of your board, the Virtual ComPort in the STM32U58I-IOT02A is connected to USART1, not USART3.

Gyessine_0-1747297837134.png

 

Thank you.

Gyessine

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Team,

Thank you for the suggestions.

I am currently planning to use both UART2 and UART3 for different operations. However, I’ve observed that transmissions on the remaining UARTs are not working as expected.

Could you please let me know what additional steps or configurations I should check to ensure proper functionality?

Looking forward to your guidance.

Gyessine
ST Employee

Hello @ram_jan 

The virtual COM port provided by the ST-Link, which allows you to print results in the serial monitor, is only connected to USART1  in your specific board . If you want to use other USARTs, such as USART2 or USART3, you will need to implement buffering since they are not directly linked to the ST-Link. You can refer to This Wiki 

Thank you

Gyessine

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks for the Suggestion, I will check and update !!!