2022-12-12 8:36 AM
Hi,
Im trying to get WUP reason after the MCU exited the shutdown. I'm using pushbutton connected to PC5 pin to wake up the MCU. I cannot get the WUP flag to behave correctly. Sometimes it is present, sometimes not. This feature is part of bigger project where I use WUP by two alarms and pushbutton. I have no problem detecting that the WUP happend due to alarmA or alarmB, but I'm struggling with the pushbutton.
Here is code snippet from test app where I am debugging behaviour of WUP:
__HAL_RCC_GPIOC_CLK_ENABLE();
HAL_UART_Transmit(&hlpuart1, "Hello\r\n", 7, 300);
if(PWR->WUSR & PWR_WUSR_WUF5)
{
PWR->WUSCR &= PWR_WUSCR_CWUF5; //clear flag
HAL_UART_Transmit(&hlpuart1, "Button WUP!\r\n", 13, 300);
}
char buff[32]="";
sprintf(buff, "WUSR:%08X, CSR:%08X\r\n",PWR->WUSR,RCC->CSR);
HAL_UART_Transmit(&hlpuart1, buff, strlen(buff), 300);
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN5);
__HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_FLAG5);
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN5_HIGH_0);
HAL_PWREx_EnterSHUTDOWNMode();
If I attach the debugger everything starts to work just fine. Is there something I am doing wrong ? Are the registers reseted upon exiting shutdown ?
2022-12-13 6:33 AM
Hello @David He�?ko and welcome to the Community :smiling_face_with_smiling_eyes:,
The Wake up flag WUF5 is cleared by writing 1 in the CWUF5 bit of PWR_WUSCR,
to do so, this is the right instruction : PWR->WUSCR |= PWR_WUSCR_CWUF5;
Thank you!
Sarra.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-12-13 7:48 AM
Hi @Sarra.S , thank you for quick response. I've tried this fix and it unfortunately does not seems to help.
2022-12-15 2:03 AM
Hello again @David He�?ko,
I am not sure if the if statement is even being executed
if(PWR->WUSR & PWR_WUSR_WUF5)
{
PWR->WUSCR &= PWR_WUSCR_CWUF5; //clear flag
HAL_UART_Transmit(&hlpuart1, "Button WUP!\r\n", 13, 300);
}
To make sure, is the "Button WUP!" string being displayed ?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-12-20 4:04 PM
No, the correct code is:
PWR->WUSCR = PWR_WUSCR_CWUF5;
Take a note that it doesn't use an OR instruction and is not a RMW (Read-Modify-Write) operation.