cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U575QII Dedicated OPAMP2_VINM pin not connected?

Tomas Hamouz
Associate III

I have a project which uses both OPAMPs. For both OA I use dedicated VINM pin.

OPAMP1 works correctly.

OPAMP2 behaves like the dedicated pin (M2 ball) is not connected to the input multiplexer.

I 've tried

 - mode FOLLOWER: OK

 - mode STANDALONE, reconnected the signal on the board and used PA7 for VINM: OK

 - mode STANDALONE, using the dedicated pin: the output is saturated at VDDA.

Checked the PCB connection, OK. Checked on 3 boards, identical results.

Is it possible it is really a bug in the silicon? What else should I check?

(I would like to use OPAMP tag, but it is not available   )

 

Initialization code:

(GPIO to analog)

LL_APB3_GRP1_EnableClock(LL_APB3_GRP1_PERIPH_OPAMP);

LL_OPAMP_InitTypeDef OPAMP_Init;

OPAMP_Init.PowerMode = LL_OPAMP_POWERMODE_NORMALPOWER_NORMALSPEED;
OPAMP_Init.FunctionalMode = LL_OPAMP_MODE_STANDALONE;
OPAMP_Init.InputNonInverting = LL_OPAMP_INPUT_NONINVERT_IO0;
OPAMP_Init.InputInverting = LL_OPAMP_INPUT_INVERT_IO1;
LL_OPAMP_Init(OPAMP2, &OPAMP_Init);

LL_OPAMP_Enable(OPAMP2);

 

 

 

 

6 REPLIES 6
Amel NASRI
ST Employee

Hi @Tomas Hamouz ,

Sorry to come back late to this question.

Do you still face an issue or you succeed to find a solution? That would be interesting to share the status.

In case you continue the investigation, could you please:

  • share the revision of the used devices
  • read the value of the bit field VM_SEL in both OPAMP1_CSR and OPAMP2_CSR

-Amel

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Tomas Hamouz
Associate III

Hi @Amel NASRI ,

Silicon revison is W, see attached picture, all devices the same. See also the snapshot of OPAMP registers from debugger.

Tomas

STM32U575_2.jpg

OPAMP_settings.PNG

Hi @Tomas Hamouz ,

Thanks for sharing these details.

Our expert made a test with a BGA169 package and OPAMP2_VINM is working properly for both modes STANDALONE & FOLLOWER.

We will try to continue investigation using a BGA132 (as it is the case for you) and will come back to you.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi @Tomas Hamouz ,

I come back to you to confirm that internal tests were performed by our team with BGA132 package.

Both OPAMP1 & OPAMP2 are configured in standalone mode with dedicated VINM pin configured and the work properly.

At this level, I recommend you to review your hardware setup. If the problem is still there, could you please share the used firmware? It may be interesting also to share your schematic.

-Amel

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi @Amel NASRI ,

Thanks for investigation, the problem persists. See the attached snippets of code, principal schematic, a cut from real board routing and X-rayed board, confirming there is not bad connection under the M2 ball.

Summary:

 - when compiled with #define TEST_FOLLOWER_ONLY, it works.

- when compiled without TEST_FOLLOWER_ONLY, the OPAMP is saturated to Vdda

- when OPAMP_VINM reconnected to PA7 and source code changed (see commented out line), it works.

When saturated, the pads 1 (C3, R32) have Vdd/2, pads 2 have VDDA.

Snippet of code here, max 3 attachments

Tomas

//-----------------------------------------------------------------------------
/// OPAMP Initialization
void CWetContacts::InitOpAmp(void)
//-----------------------------------------------------------------------------
{
LL_APB3_GRP1_EnableClock(LL_APB3_GRP1_PERIPH_OPAMP);

// GPIO setup
LL_GPIO_InitTypeDef GPIO_InitStruct;

// minus need not setup, BGA132 has dedicated pin
// plus PA6
// output PB0
GPIO_InitStruct.Pin = WET_OPAMP_INP_PLUS_PIN;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(WET_OPAMP_INP_PLUS_PORT, &GPIO_InitStruct);

GPIO_InitStruct.Pin = WET_OPAMP_OUT_PIN;
LL_GPIO_Init(WET_OPAMP_OUT_PORT, &GPIO_InitStruct);

// configuration of OPAMP
LL_OPAMP_InitTypeDef OPAMP_Init;
LL_OPAMP_StructInit(&OPAMP_Init);

OPAMP_Init.PowerMode = LL_OPAMP_POWERMODE_NORMALPOWER_NORMALSPEED;
OPAMP_Init.InputNonInverting = LL_OPAMP_INPUT_NONINVERT_IO0; // std gpio pin

#if defined(TEST_FOLLOWER_ONLY)
OPAMP_Init.FunctionalMode = LL_OPAMP_MODE_FOLLOWER;
OPAMP_Init.InputInverting = LL_OPAMP_INPUT_INVERT_CONNECT_NO; // minus need not connection
#else // !defined(TEST_FOLLOWER_ONLY)
OPAMP_Init.FunctionalMode = LL_OPAMP_MODE_STANDALONE; // amplification by external circuit
OPAMP_Init.InputInverting = LL_OPAMP_INPUT_INVERT_IO1; // dedicated pin
// OPAMP_Init.InputInverting = LL_OPAMP_INPUT_INVERT_IO0; // test alternate pin PA7
#endif // !defined(TEST_FOLLOWER_ONLY)
LL_OPAMP_Init(WET_OPAMP_DEVICE, &OPAMP_Init);

LL_OPAMP_Enable(WET_OPAMP_DEVICE);
} // InitOpAmp

 

 

 

STM32U575QII6Q_OPAMP2_pcb.png

STM32U575QII6Q_OPAMP2_sch.png

STM32U575QII6Q-OPAMP-_rtg.jpg

   

 

 

Hello @Tomas Hamouz ,

No weird setup based on what you shared.

What I suggest at this level is to contact your FAE who can make checks with your hardware to reproduce issue and go farther with the analysis. Please let me know if you opt for this.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.