2025-01-09 06:29 AM
Hello, is there any possibility to get the pin configuration table for the STM32U535VE in CSV or Excel format?
Thanks a lot !
Ricos
2025-01-09 06:53 AM
Yes, it would be really useful if the pinout table, alternate function table, etc were made available in an easy machine-readable format - rather than just as text in the Datasheet & Ref Manual.
I'm sure I've requested this before.
One thing you can do is to create a project in CubeMX, and then use Project > Generate Report
Or the IBIS files will give you a start - with pin number & name; eg,
|************************************************************************
| stm32f0_440_lqfp32 IBIS Model
|************************************************************************
[IBIS ver] 4.2
[File name] stm32f0_440_lqfp32.ibs
[File Rev] 1.0
[Date] 15-5-2013
[Source] Data Created at STMicroelectronics
[Notes] File originated from ELDO simulations.
[Disclaimer] This information is for modeling purpose only and is
not guaranted. The information is subject to change without
notice.
[Copyright] Copyright 2015 STMicroelectronics Inc.
|
[Component] stm32f0_440_lqfp32
[Manufacturer] STMicroelectronics
[Package]
| variable typ min max
R_pkg 0.0 NA NA
L_pkg 0.0H NA NA
C_pkg 0.0F NA NA
|
[Pin] signal_name model_name R_pin L_pin C_pin
1 VDD POWER 0.03449 2.11E-09 6E-14
2 PF0 io8p_sudq_ft 0.029020556 1.54333E-09 3.22222E-14
3 PF1 io8p_sudq_ft 0.025738889 1.20333E-09 1.55556E-14
4 NRST ioreset_tc_v33 0.024645 1.09E-09 1E-14
5 VDDA POWER 0.024645 1.09E-09 1E-14
6 PA0 io8p_sudq_ft 0.025738889 1.20333E-09 1.55556E-14
7 PA1 io8p_sudq_ft 0.029020556 1.54333E-09 3.22222E-14
8 PA2 io8p_sudq_ft 0.03449 2.11E-09 6E-14
9 PA3 io8p_sudq_ft 0.03449 2.11E-09 6E-14
10 PA4 io8p_sudq_ft 0.029020556 1.54333E-09 3.22222E-14
11 PA5 io8p_sudq_ft 0.025738889 1.20333E-09 1.55556E-14
12 PA6 io8p_sudq_ft 0.024645 1.09E-09 1E-14
13 PA7 io8p_sudq_ft 0.024645 1.09E-09 1E-14
14 PB0 io8p_sudq_ft 0.025738889 1.20333E-09 1.55556E-14
15 PB1 io8p_sudq_ft 0.029020556 1.54333E-09 3.22222E-14
16 VSS GND 0.03449 2.11E-09 6E-14
17 VDD POWER 0.03449 2.11E-09 6E-14
18 PA8 io8p_sudq_ft 0.029020556 1.54333E-09 3.22222E-14
19 PA9 io8p_sudq_ft 0.025738889 1.20333E-09 1.55556E-14
20 PA10 io8p_sudq_ft 0.024645 1.09E-09 1E-14
21 PA11 io8p_sudq_ft 0.024645 1.09E-09 1E-14
22 PA12 io8p_sudq_ft 0.025738889 1.20333E-09 1.55556E-14
23 PA13 io8p_sudq_ft 0.029020556 1.54333E-09 3.22222E-14
24 PA14 io8p_sudq_ft 0.03449 2.11E-09 6E-14
25 PA15 io8p_sudq_ft 0.03449 2.11E-09 6E-14
26 PB3 io8p_sudq_ft 0.029020556 1.54333E-09 3.22222E-14
27 PB4 io8p_sudq_ft 0.025738889 1.20333E-09 1.55556E-14
28 PB5 io8p_sudq_ft 0.024645 1.09E-09 1E-14
29 PB6 io8p_sudq_i2cin_lv_ft 0.024645 1.09E-09 1E-14
30 PB7 io8p_sudq_i2cin_lv_ft 0.025738889 1.20333E-09 1.55556E-14
31 BOOT0 vpp_test_hv 0.029020556 1.54333E-09 3.22222E-14
32 VSS GND 0.03449 2.11E-09 6E-14
2025-01-09 07:52 AM
Thanks Andrew. In my work I only define the functions of the pins, so such a table is suitable to provide results. I hope ST can provide a table as useful as other providers already do.
2025-01-10 01:55 AM
@RicOs wrote:a table as useful as other providers already do.
Out of interest, which other providers have you found which do that?