2026-04-20 8:03 AM - last edited on 2026-04-20 8:08 AM by Andrew Neil
Hi,
I am using STM32U385CGU6 with 1.8V supply. My GSM peripheral using the 3.3V Uart port for a dedicated time (2sec) then turn back to 1.8V level of UART.
Could you offer 3.3V tolerant pin? I am using PA8 to communicate with GSM module.
thank you & best regards,
feramuz karşil
Solved! Go to Solution.
2026-04-20 8:46 AM
Look at pin/ball definitions table in Datasheet, that lists all pins together with their input/output structure.
Now look at General operating conditions table, that gives the permissible range of voltages for each type of pin. For TT_xx pins, it's generally up to its VDDIO (which except some PGx pins and USB pins is identical to VDD) supply voltage; for FT_xx pins ("five-volt tolerant"), it's up generally up to VDDIO+3.6V or 5.5V, whichever is less.
PA8 is listed as FT_h, so it should be OK if it is turned to input and 3.3V is applied to it. It won't be able to source 3.3V when VDD is 1.8V, though.
JW
2026-04-20 8:37 AM - edited 2026-04-20 8:43 AM
Hello,
From the datasheet (DS14830 - Rev 3) / Table 27. General operating conditions
That depends on what you are using as power supply.
2026-04-20 8:46 AM
Look at pin/ball definitions table in Datasheet, that lists all pins together with their input/output structure.
Now look at General operating conditions table, that gives the permissible range of voltages for each type of pin. For TT_xx pins, it's generally up to its VDDIO (which except some PGx pins and USB pins is identical to VDD) supply voltage; for FT_xx pins ("five-volt tolerant"), it's up generally up to VDDIO+3.6V or 5.5V, whichever is less.
PA8 is listed as FT_h, so it should be OK if it is turned to input and 3.3V is applied to it. It won't be able to source 3.3V when VDD is 1.8V, though.
JW
2026-04-20 9:21 AM
Hi JW,
thank you for your feedback.
best regards,