2025-07-08 8:56 AM - last edited on 2025-08-27 7:18 AM by KDJEM.1
Hello, I get the same error recently on 1.19.0 for my STM32U385RGTxQ. The only option available in Power Supply source is PWR_LDO_SUPPLY
Solved! Go to Solution.
2025-12-01 12:30 AM
Hello @george-metasphere and @C_G ;
The issue is fixed in STM32CubeMX 6.16.0 version.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-13 7:09 PM
Having the same issue as George-methasphere.
Can't find anywhere to include the smps in the drop down list of the RRC> Parameter Settings>Power Parameters>SuppySource STM32U385RGTxQ using STM32CUBEIDE v1.19.0 with STM32Cube MCU package for stm32U3 Series 1.2.0
2025-08-27 7:19 AM
Hello @george-metasphere and @C_G ;
This post has been moved from Solved: STM32U5 invalid SMPS warning during code generatio... - STMicroelectronics Community
Thank you for bringing this issue to our attention.
I reported internally.
Internal ticket number: 214214 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-12-01 12:30 AM
Hello @george-metasphere and @C_G ;
The issue is fixed in STM32CubeMX 6.16.0 version.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.