cancel
Showing results for 
Search instead for 
Did you mean: 

STM32SnippetsL0 TIMER examples bug

Posted on August 16, 2017 at 17:33

In TIMERS/03_InputCapureOnTI1/main.c and TIMERS/04_PWM_Input/main.c the flags after an interrupt are being cleared this way:

TIMx->SR = ~(TIM_SR_CC1OF | TIM_SR_CC1IF); /* Clear the flags */

Shouldn't it be like below?

TIMx->SR &= ~(TIM_SR_CC1OF | TIM_SR_CC1IF); /* Clear the flags */

#timer #stm32snippetsl0 #bug
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Radosław
Senior III
Posted on August 16, 2017 at 18:22

No,  version with and is wrong.  RMW operation for clearing flags is very bad idea.

View solution in original post

5 REPLIES 5
Radosław
Senior III
Posted on August 16, 2017 at 18:22

No,  version with and is wrong.  RMW operation for clearing flags is very bad idea.

Posted on August 16, 2017 at 19:18

No this is a recurrent issue because people don't read and understand the manual and implementation.

RMW creates a hazard, it is not atomic, and the TIM can go through several cycles between the read and write operations.

Bit-Banding the TIM->SR is also highly hazardous, again not atomic from the peripherals perspective.

A singular write is contained to a cycle of the TIM.

The peripheral registers should not be viewed a memory cells, but as combinational logic.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on August 16, 2017 at 19:28

From the user point of view: if a register bit is marked as rc_w0 (or rc_w1) in the RM, it means extra circuitry which is there for a reason...

J\W

Posted on August 16, 2017 at 19:40

I've covered this in multiple threads over many years, but ..

The nature of the hazard is when you AND something with ZERO it becomes ZERO, and you have a race condition here where the initial read of the SR might have a number of interrupts flagged as ZERO, and these bits may subsequently flag as ONE, and the RMW form will stomp on them, indiscriminately.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on August 17, 2017 at 10:50

Thank you, now I understand the advantage of the fact that writing 1 into a bit marked as rc_w0 (or writing 0 into rc_w1) is ignored and this is how one issues atomic writes with changing only the desired bits without touching the others, instead of doing a RMW.