2022-03-03 5:15 AM
Hi STM32-Community,
I'm currently using an STM32L4R-MCU and was trying to set it up for standby. By using LoRa, I don't want it to keep requesting an OTAA-Command to join the network, I'm trying to use the SRAM2 Retention of my MCU in Standby-Mode. Googling and skimming through the datasheet, I only found at which adress the 64 KB SRAM are located, but how do I actually write to that memory and also read it back again?
I've neither found an application note, nor an example code. I would be really glad, if someone knows more about this topic.
Kind regards
crackl1ng
Solved! Go to Solution.
2022-03-04 5:39 AM
I think I have understood it now.
For anyone wondering:
There is a .ld.file, in which the linker gets told, where it should save its data. You have to add RAM2 eg if you want to use SRAM2.
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 640K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 2048K
RAM2 (xrw) : ORIGIN = 0x10000000, LENGTH = 64K
}
followed by
.ram2 (NOLOAD):
{
_sram2 = .;
*(.ram2*)
. = ALIGN(4);
_eram2 = .;
} >RAM2
Followed by this in the SECTIONS part.
Now data can be initialized within SRAM2 like this:
volatile uint32_t Counter __attribute__((section(".ram2")));
volatile uint32_t test123[20] __attribute__((section(".ram2")));
Et voilà:
I saved n³ (for n from 0 to 19) in test123, and counter was reset on purpose.
Thank you very much for your post, it helped me a lot!
Kind regards
2022-03-03 5:52 AM
Set up a segment in your linker script for SRAM2 and assign variables to be placed there, or create a pointer to that memory and store them manually.
Follow this, but use SRAM2 instead of CCMRAM:
https://www.openstm32.org/Using%2BCCM%2BMemory
2022-03-04 1:35 AM
Thank you for your reply. That looks very promising and I will try it out. Anyway, there is no application note directly from STM32? Those always have been very informative and usually worked flawlessly.
2022-03-04 5:39 AM
I think I have understood it now.
For anyone wondering:
There is a .ld.file, in which the linker gets told, where it should save its data. You have to add RAM2 eg if you want to use SRAM2.
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 640K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 2048K
RAM2 (xrw) : ORIGIN = 0x10000000, LENGTH = 64K
}
followed by
.ram2 (NOLOAD):
{
_sram2 = .;
*(.ram2*)
. = ALIGN(4);
_eram2 = .;
} >RAM2
Followed by this in the SECTIONS part.
Now data can be initialized within SRAM2 like this:
volatile uint32_t Counter __attribute__((section(".ram2")));
volatile uint32_t test123[20] __attribute__((section(".ram2")));
Et voilà:
I saved n³ (for n from 0 to 19) in test123, and counter was reset on purpose.
Thank you very much for your post, it helped me a lot!
Kind regards
2024-04-11 7:04 AM
Hello there,
Did you find a solution to store the context in SRAM ? For not rejoining the context ?
I'm struggling with the ST example and the NVM management.
Can you share you're solution or some tips?
Have a good day
Anthony