cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L476xx disambiguation

Noyb
Associate II
Posted on May 18, 2016 at 15:53

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
19 REPLIES 19
Posted on May 18, 2016 at 17:04

These are things you'd perhaps want to discuss with the FAE assigned to your project, this is primarily a user forum, and not one the IC designers, software engineers or technical writers service.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Noyb
Associate II
Posted on May 18, 2016 at 17:24

Nope, no FAE or whatever you call it assigned to my project. Using publicly available document and material, obviously not in final revision. Btw...

Case 4 (CCMR3) :

Solved (between OR1 and CCR5)

Case 21 :

stm32l476xx.h, l520

FMC_Bank1_TypeDef, BTCR register

This register is not described into the documentation and the header file.

Case 22 :

stm32l476xx.h, l529

FMC_Bank1E_TypeDef, BWTR register

stm32l476xx.h, l4372

/******************  Bit definition for FMC_BWTRx registers (x=1..4)  *********/

en.DM00083560.pdf, p379

Bit 14 EXTMOD: Extended mode enable

This register is not described into the documentation.

Case 23 :

en.DM00083560.pdf, p440

ADDIS=1 disables the ADC and disable the ADC. ADEN and ADDIS are then automatically cleared by hardware as soon as the analog ADC is effectively disabled.

disables the ADC

and disable the ADC

...

Case 24 :

en.DM00083560.pdf, p440

Once DEEPPWD=0 and ADVREGRN=1, the ADC can be enabled and the ADC...

The register ADVREGRN is not described into the documentation.

Do you mean ADVREGEN ?

Case 25 :

en.DM00083560.pdf, p436

The software must wait for the startup time of the ADC voltage regulator (TADCVREG_STUP, =20us) before launching a calibration or enabling the ADC.

en.DM00083560.pdf, p440

...the ADC can be enabled and the ADC needs a stabilization time of tSTAB (DAC, not ADC, =5 us) before it starts converting accurately...

So, which tempo is correct ?

Case 26 :

en.DM00083560.pdf, p45

Table 56. FMC_BCRx bit fields . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 355

Table 57. FMC_BTRx bit fields. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 356

Table 58. FMC_BCRx bit fields . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 358

Table 59. FMC_BTRx bit fields. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 358

Table 60. FMC_BWTRx bit fields . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 359

Table 61. FMC_BCRx bit fields . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 361

Table 62. FMC_BTRx bit fields. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 361

Table 63. FMC_BWTRx bit fields . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 362

Table 64. FMC_BCRx bit fields . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 363

Table 65. FMC_BTRx bit fields. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 364

Table 66. FMC_BWTRx bit fields . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 364

Table 67. FMC_BCRx bit fields . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 366

Table 68. FMC_BTRx bit fields. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 366

Table 69. FMC_BWTRx bit fields . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 367

Table 70. FMC_BCRx bit fields . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 368

Table 71. FMC_BTRx bit fields. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 369

Table 72. FMC_BCRx bit fields . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 374

Table 73. FMC_BTRx bit fields. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 375

Table 74. FMC_BCRx bit fields . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 376

Table 75. FMC_BTRx bit fields. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 377

Seriously, can't you sum it up in a table with rows and columns for better comparison ?

Posted on May 18, 2016 at 19:52

Ok, just saying, because I don't think this is going to get much attention/traction in this venue.

I'll point out that the USB stuff has historically used Third Party IP (

http://www.synopsys.com/IP/InterfaceIP/USB/Pages/default.aspx

), and there are likely NDAs around register level documentation with that.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on May 18, 2016 at 19:57

FAE - Field Application Engineer

Working either for the distributor of your parts (Arrow, Farnell, etc) or ST
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Noyb
Associate II
Posted on May 19, 2016 at 11:08

Case 27 :

stm32l476xx.h, l332

  __IO uint8_t  IDR;         /*!< CRC Independent data register,               Address offset: 0x04 */

en.DM00083560.pdf, p340

Bits 31:0 IDR[31:0]: General-purpose 32-bit data register bits

So, 8 bits or 32 bits ? Get your facts straight, for God's sake !
waclawek.jan
Super User
Posted on May 19, 2016 at 11:27

IMO it's more useful to refer to DS/RM by its number and revision, rather than filename.

Thus, in RM0351 rev.1, CRC_IDR was indeed quoted to be 8-bit. Probably an omission corrected in DS, not in the header.

It's a shame the key header(s) is(are) in such a state. Mayla, Syrine or anybody other of ST listening here, could you please push this as a Cube issue? I presume it gets higher priority than general rants these days. I'd also like to reiterate my request to add bitfield-value constants/defines to these headers.

JW

Walid FTITI_O
Senior II
Posted on May 19, 2016 at 15:49

Hi Noyb,

Thanks for your contribution and feedbacks. Some of them are relevant and other ones are not (see example below).

Like:

Case 5 :

 

 

stm32l476xx.h, l1053

 

USB_OTG_GlobalTypeDef, HNPTXSTS register

 

 

en.DM00083560.pdf, p1541

 

43.15.11 OTG non-periodic transmit FIFO/queue status register (OTG_HNPTXSTS)

 

 

in stm32l476xx.h, it is written :

/*!<  Non Periodic Tx FIFO/Queue Sts reg           02Ch*/

-> It is OK.

I will report relevant ones internally for check.

-Hannibal-
Walid FTITI_O
Senior II
Posted on May 19, 2016 at 15:51

Hi waclawek.jan,

''I'd also like to reiterate my request to add bitfield-value constants/defines to these headers''

 

 

Can you give us a refresh about this request ( any reference thread for example) ?

-Hannibal-

Walid FTITI_O
Senior II
Posted on May 19, 2016 at 16:34

Hi Noyb, 

An answer to your question in one of the irrelevant feedbacks (case 25):

Case 25 :

 

en.DM00083560.pdf, p436

 

The software must wait for the startup time of the ADC voltage regulator (TADCVREG_STUP, =20us) before launching a calibration or enabling the ADC.

 

en.DM00083560.pdf, p440

 

...the ADC can be enabled and the ADC needs a stabilization time of tSTAB (DAC, not ADC, =5 us) before it starts converting accurately...

 

So, which tempo is correct ?

-> You can figure out the difference from reference manual :

''(T

ADCVREG_STUP

) before launching a calibration or enabling the ADC. This delay must be implemented by software''. -> delay (ADC voltage regulator statup time) before you can enable the ADC or launch

calibration

.

''the ADC can be enabled and the ADC needs a stabilization time of t

STAB

before it starts converting accurately'' -> delay after enabling ADC and before starting conversion

-Hannibal-