2022-03-04 1:36 AM
That is what I send for exsample:
SIR 9 TDI (0);
SDR 334 TDI (49000000001249240a49249248000000000001249200000000000249249249008000000001249200) SMASK (3fffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffff) TDO (0) MASK (0);
Solved! Go to Solution.
2022-04-01 7:33 AM
Hello,
I confirm that there is an issue with the STM32L451_LQFP64.bsd package, thanks for bringing it to our attention..
An internal ticket number 125629 (This is an internal tracking number and is not accessible or usable by customers) has be logged to check all the other packages.
Please find attached an updated version of the needed file.
Please note that an updated version of the file en.stm32l4_bsdl will be available on ST website.
2022-03-23 2:52 AM
Hello,
Can you please precise the package you're using?
Br,
2022-03-23 3:39 AM
Package is LQFP64
I Took the BSDL File for the Package STM32L451_LQFP64.bsd and than the Cortex
2022-03-29 1:06 AM
Hello,
The BSDL chain length is 234 bits long. And it seems that you're shifting 334 bits
Can you check that? an is the STM32 daisy-chained with other devices?
Br,
2022-03-29 3:34 AM
Thank you for your Answer, it is difficult to check without the right BSDL File. I use the File witch is available at the st homepage like specified before, with the zip File en.stm32l4_bsdl. Downloaded a few Weeks before. In the bsdl File the JTAG Interface is specified with 333 Cells (0 till 332). The File is dated with 09-May-2017. Obviously you have an other BSDL File. Can you provide a link to the File? There are no other devices in the scan chain (Except the Cortex TAP).
2022-04-01 7:33 AM
Hello,
I confirm that there is an issue with the STM32L451_LQFP64.bsd package, thanks for bringing it to our attention..
An internal ticket number 125629 (This is an internal tracking number and is not accessible or usable by customers) has be logged to check all the other packages.
Please find attached an updated version of the needed file.
Please note that an updated version of the file en.stm32l4_bsdl will be available on ST website.
2022-04-06 5:20 AM
Thank you for your support!!!