Hello,Actually the choice of the needed submodel depends on your use case. Below you can find some clarifications about the models:IO speed: speed00: low speed, speed01: medium, speed10: high, speed11: very highpd: pull down, pu: pull upBest regards,
Hello TSang.3,In the "On the Interpretation of Results from the NIST Statistical Test Suite" it shows that data can be considered random even if it does not pass all the tests :"Computed reference cumulative probabilities indicate that a single seque...
Hello,I confirm that there is an issue with the STM32L451_LQFP64.bsd package, thanks for bringing it to our attention..An internal ticket number 125629 (This is an internal tracking number and is not accessible or usable by customers) has be logged ...
Hello,The BSDL chain length is 234 bits long. And it seems that you're shifting 334 bitsCan you check that? an is the STM32 daisy-chained with other devices? Br,