cancel
Showing results for 
Search instead for 
Did you mean: 

[STM32L4] timer interrupt starts immediately

Noyb
Associate II
Posted on October 04, 2016 at 13:07

Hi, using TIM1 to get a simple 1ms delay (MCU@24MHz, PSC=24, ARR=1000) the interrupt triggers almost as soon as I set CR1:CEN=1.

I've found that I'm not the only one having this problem, have followed the advice given here and there, but still no luck.

1- Start peripheral (RCC)

2- Reset peripheral

3- Set registers (SR, CR1, SMCR, BDTR, CNT, ARR, PSC)

4- Do some read back to ensure propagation

5- Tried the EGR:UG=1 trick

6- Tried the CR1:URS=1 trick

7- Interrupt is cleared at the beginning of the ISR

8- Start the timer, interrupt triggers within 50us (about 1200 cycles)

This is rather hard to get this thing working without deploying a whole army.

#stm32l4-timer-interrupt-spurious #stm32l4-timer-interrupt-spurious #stm32l4-timer-interrupt-spurious #stm32l4-timer-interrupt-spurious #stm32l4-timer-interrupt-spurious
9 REPLIES 9
Posted on October 04, 2016 at 13:24

Which interrupt?

Post code.

JW

Noyb
Associate II
Posted on October 04, 2016 at 14:11

Can' post code, too complicated, not MX stuff, scattered all over several files.

1- RCC->APB2ENR |= RCC_APB2ENR_TIM1EN

2- RCC->APB2RSTR |= RCC_APB2RSTR_TIM1RST

3- RCC->APB2RSTR &= ~RCC_APB2RSTR_TIM1RST

4- TIM->CR1 |= (TIM_CR1_URS) (trick ?)

5- TIM->SR = 0, tim_sr = TIM->SR (read back)

6- TIM->CR1 = 0

7- TIM->SMCR = 0

8- TIM->BDTR = TIM_BDTR_MOE

9- TIM->CNT = 0

10- TIM->ARR = 1000 - 1 (1000us)

11- TIM->PSC = 24 - 1, tim_psc = TIM->PSC (read back)

12- TIM->RCR = 0

13- TIM->EGR &= TIM_EGR_UG (trick ?)

14- TIM->DIER = TIM_DIER_UIE

15- NVIC_ClearPendingIRQ(TIM1_UP_TIM16_IRQn) & (TIM1_CC_IRQn)

16- NVIC_SetPriority(TIM1_UP_TIM16_IRQn) & (TIM1_CC_IRQn)

17- NVIC_EnableIRQ(TIM1_UP_TIM16_IRQn) & (TIM1_CC_IRQn) -> could triggers here

18- TIM->CR1 &= ~(TIM_CR1_URS) (trick ?)

19- TIM->CR1 |= (TIM_CR1_OPM)

20- TIM->SR = 0, tim_sr = TIM->SR (yeah, to be sure)

21- TIM->CR1 |= (TIM_CR1_CEN)

22- Boom! after 50us instead of 1000us :/

Posted on October 04, 2016 at 14:26

> TIM->EGR &= TIM_EGR_UG (trick ?)

No, this won't do the trick. You need to *set* TIM_EGR.UG.

JW

Posted on October 04, 2016 at 15:43

> TIM->EGR &= TIM_EGR_UG (trick ?)

No, this won't do the trick. You need to *set* TIM_EGR.UG.

JW
Noyb
Associate II
Posted on October 04, 2016 at 15:49

Could you post your correction to my code flow?

Posted on October 04, 2016 at 16:05

> Could you post your correction to my code flow?

>>> TIM->EGR &= TIM_EGR_UG (trick ?)

>> No, this won't do the trick. You need to *set* TIM_EGR.UG.

TIM->EGR = TIM_EGR_UG;

JW

Noyb
Associate II
Posted on October 04, 2016 at 16:45

Nope, doesn't work, already tried that.

It appears that the counter doesn't even start counting when CR1:CEN=1 because when reading CNT it remains at 0. However the interrupt is triggered just after that.

When using TIM3 CH4 for PWM, no problem, CNT runs fine after CR1:CEN=1 :/

Posted on October 04, 2016 at 17:07

> Nope, doesn't work, already tried that.

WHAT doesn't work? What did you try already?

> It appears that the counter doesn't even start counting when CR1:CEN=1 because when reading CNT it remains at 0.

Reading how? Can't this be because of the one-pulse mode you set?

Create a simple but complete, compilable example reproducing the problem, and post that.

Noyb
Associate II
Posted on October 05, 2016 at 12:04

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6ke&d=%2Fa%2F0X0000000buc%2FIvtdbxP5krhSW3eBRJvPcph8tT17N3ek3ygUIMXhWgU&asPdf=false