STM32L4 Pin State in shutdown mode
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-04 7:43 AM
We are trying to set the STM32L431 controller to shutdown mode.
During the shutdown mode, Pin PA15 shall be at low level.
Unfortunately the pin does not stay at low level during shutdown.
We have configured the pin with „HAL_PWREx_EnableGPIOPullDown(PWR_GPIO_A, PWR_GPIO_BIT_15);“
Because PA15 is a JTAG pin and equipped with internal pull-ups during reset i am searching the problem there.
Do I use the wrong pin configuration or is it not possible to achive a low level on PA15 in shutdown?
Thank you
- Labels:
-
GPIO-EXTI
-
STM32L4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-04 9:39 PM
RM0351 says:
"I/O states in Shutdown mode
In the Shutdown mode, the I/Os can be configured either with a pull-up (refer to
PWR_PUCRx registers (x=A,B,C,D,E,F,G,H), or with a pull-down (refer to PWR_PDCRx
registers (x=A,B,C,D,E,F,G,H)), or can be kept in analog state. However this configuration is
lost when exiting the Shutdown mode due to the power-on reset.
The RTC outputs on PC13 are functional in Shutdown mode. PC14 and PC15 used for LSE
are also functional. 5 wakeup pins (WKUPx, x=1,2...5) and the 3 RTC tampers are available."
I guess the ports are in high Z state, but the pull-ups/downs are there.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-04 11:02 PM
Yes I have seein this section in the manual.
I just found out why it was not working on my controller. During debugging all pins assigned to JTAG behave a bit different. If I startup the system without debug connection, everything is working fine.