cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L151 SPI1 Problem

arulprabhu
Associate II
Posted on January 12, 2013 at 06:44

Hi clive,

I have a started a new thread for discussion about SPI1 problem in STM32L151.

I used PA4-A7 for SPI1

This is my SPI configuration code,

My system clock is HSE  and it is 8MHZ.

There is a continuous reset happens when the SPI transfer starts,

Can anyone find the problem,

void RCC_config(void)

 {

    ErrorStatus HSEStartUpStatus;

    /* RCC system reset(for debug purpose) */

    RCC_DeInit();

    /* Enable HSE */

    RCC_HSEConfig(RCC_HSE_ON);

    /* Wait till HSE is ready */

    HSEStartUpStatus = RCC_WaitForHSEStartUp();

    if (HSEStartUpStatus == SUCCESS)

    {

        /* HCLK = SYSCLK */

        RCC_HCLKConfig(RCC_SYSCLK_Div1);

        /* PCLK2 = HCLK */

        RCC_PCLK2Config(RCC_HCLK_Div2);

        /* PCLK1 = HCLK/2 */

        RCC_PCLK1Config(RCC_HCLK_Div2);

            

            

            

           PWR_VoltageScalingConfig(PWR_VoltageScaling_Range1);

   

       RCC_PLLCmd(DISABLE);

 

       /* Wait till HSE is ready */

        while (RCC_GetFlagStatus(RCC_FLAG_HSERDY) == RESET)

        {

        }

         RCC_SYSCLKConfig(RCC_SYSCLKSource_HSE);     // 8MHz   

        /* Wait till HSE is used as system clock source */

        while (RCC_GetSYSCLKSource() != 0x08)

        {

        }

      

     

      

      RCC_AHBPeriphClockCmd ( RCC_AHBPeriph_GPIOA|RCC_AHBPeriph_GPIOB, ENABLE);

        RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1 , ENABLE);

 }

}

SPI configuration code:

 GPIO_InitTypeDef  GPIO_InitStructure;

  SPI_InitTypeDef   SPI_InitStructure;

    

    SPI_I2S_DeInit(SPI1);

     

    

      RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);

    

    

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_PuPd  = GPIO_PuPd_DOWN;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

    

    

    

    

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

    

    GPIO_SetBits(GPIOA, GPIO_Pin_4);

    

        

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_SPI1);

 

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_SPI1);

 

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_SPI1);

 

 

 

    

  /*!< SD_SPI Config */

  SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

  SPI_InitStructure.SPI_Mode = SPI_Mode_Master;

  SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;

  SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;

  SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;

  SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;

  SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_128;

  SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;

  SPI_InitStructure.SPI_CRCPolynomial = 7;

  SPI_Init(SPI1, &SPI_InitStructure);

 

  SPI_Cmd(SPI1, ENABLE);

#spi1-cause-continuous-reset
0 REPLIES 0