cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L151 I2C in low power run mode

EmbeddedChris
Associate II
Posted on June 21, 2017 at 10:39

I'm looking to use the STM32L151 in low-power run mode with I2C. The datasheet says I2C can be used in this mode (DocID022799 pg.17) but to operate in low-power run mode, the system clock needs to be the MSI set to 131kHz (DocID022799 pg.14). The problem is that the reference manual says the peripheral input clock for the I2C needs to be at least 2MHz (RM0038 pg. 668) and the HAL checks for this. What am I missing here?

#stm32l1 #low-power #i2c #low-power #clock #stm32l1-i2c
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0