2015-06-08 1:43 AM
Hello
STM32L0 CUBE pack, file stm32l0xx_hal_gpio.c have a mega-bug. When will be used GPIO EXTI function, at end of config the all SYSCFG->EXTICR registers will be set to FFFF.in file, function HAL_GPIO_Init:259: temp &= ~((uint32_t)0x0F) << (4 * (position & 0x03));must be:259: temp &= ~(((uint32_t)0x0F) << (4 * (position & 0x03)));This bug may have place in the other packs, need to check it.To developers: People, please adjust it in your sources and archives!!!2015-06-11 2:58 AM
Hi Elik,
This issue is already fixed in STM32CubeL0 1.2.0 that will be available soon on the web.Thanks-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.