2015-06-11 2:33 AM
Hi folks,
I was looking at the generated code from STM Cube @ STMCubeGeneratedCode\Drivers\STM32F2xx_HAL_Driver\Src\stm32fxx_hal_uart.c, UART_WaitOnFlagUntilTimeout() below. According to the comment of the code, the Status is meant for the new Status of the flag, however if you look at the code below, the algorithm seems to be doing the opposite(due to the while loop expression)./**
* @brief This function handles UART Communication Timeout. * @param huart: UART handle * @param Flag: specifies the UART flag to check. * @paramStatus
:The new Flag status (SET or RESET).
* @param Timeout: Timeout duration * @retval HAL status */ static HAL_StatusTypeDef UART_WaitOnFlagUntilTimeout(UART_HandleTypeDef *huart, uint32_t Flag, FlagStatusStatus
, uint32_t Timeout) { uint32_t timeout = 0; timeout = HAL_GetTick() + Timeout; /* Wait until flag is set */ if(Status == RESET
) { while(__HAL_UART_GET_FLAG(huart, Flag) ==RESET
) { /* Check for the Timeout */ if(Timeout != HAL_MAX_DELAY) { if(HAL_GetTick() >= timeout) { /* Disable TXE, RXNE, PE and ERR (Frame error, noise error, overrun error) interrupts for the interrupt process */ __HAL_UART_DISABLE_IT(huart, UART_IT_TXE); __HAL_UART_DISABLE_IT(huart, UART_IT_RXNE); __HAL_UART_DISABLE_IT(huart, UART_IT_PE); __HAL_UART_DISABLE_IT(huart, UART_IT_ERR);huart->State= HAL_UART_STATE_READY;
/* Process Unlocked */
__HAL_UNLOCK(huart);return HAL_TIMEOUT;
} } } } else { while(__HAL_UART_GET_FLAG(huart, Flag) != RESET) { /* Check for the Timeout */ if(Timeout != HAL_MAX_DELAY) { if(HAL_GetTick() >= timeout) { /* Disable TXE, RXNE, PE and ERR (Frame error, noise error, overrun error) interrupts for the interrupt process */ __HAL_UART_DISABLE_IT(huart, UART_IT_TXE); __HAL_UART_DISABLE_IT(huart, UART_IT_RXNE); __HAL_UART_DISABLE_IT(huart, UART_IT_PE); __HAL_UART_DISABLE_IT(huart, UART_IT_ERR);huart->State= HAL_UART_STATE_READY;
/* Process Unlocked */
__HAL_UNLOCK(huart); return HAL_TIMEOUT; } } } } return HAL_OK; }