cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L082 - IWDG - freeze downcounter in low power possible?

Jeroen deBuffel
Associate III

Hi,

I am using the STM32L082 and looking for ways to have a watchdog implemented.

However during long periods of low power sleeps (e.g. 12 hours) I would like to freeze the IWDG downcounter.

Is this possible for the STM32L082?

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
FBL
ST Employee

Hi @Jeroen deBuffel​ 

Indeed, it is possible to freeze IWDG downcounter in low power mode. To do so, you need to enable Window Option. You may refer to the reference manual for more details. For code example, refer to A.13.2: IWDG configuration with window code example.

Note: after updating the prescaler and/or the reload/window value, there is no need to wait until RVU or PVU or WVU is reset before continuing code execution in case of low-power mode entry

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL