cancel
Showing results for 
Search instead for 
Did you mean: 

stm32l053r8 smbus

Mreva.1656
Associate

hi,

my self Revanth im using bq40z50 which Supports Two-Wire SMBus v1.1 i want to integrate this with stm32l053r8 in the data sheet it was mentiond as it will support for smbus 2.0 so will it support for smbus v1.1 as well ??? can anyone help me with this...

2 REPLIES 2
TDK
Guru

Almost certainly, the standard is backwards compatible, or at least the subset of functions that you use.

Can dig into it more here if you're interested.

http://smbus.org/specs/

If you feel a post has answered your question, please click "Accept as Solution".

If you have the parts you can undoubtedly validate this for yourself.

Pull some of the SMBUS examples for the L0 platform and port them to your board / implementation.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..