2020-05-25 3:08 AM
In the document UM1775 there is stated the following:
"5 V and 3 V can be used as output power supplies when an extension board is
connected to pins P2 and P3.
...
In this case, the 5V_O and 3V_O pins deliver a 5 V or 3.3 V power supply and the
power consumption of the extension board must be lower than 100 mA."
Yet, the Supply for 3V_O is gated through T2 which in turn is controlled by PB15 on the SM32F103 (PWR_ENn); I guess that this is the controller which handles the ST-Link and cannot be changed.
How does this controller determine if there is an extension board connected to P2 or P3 so that it enables that supply?
Solved! Go to Solution.
2020-05-25 3:43 AM
PWR_ENn enables power to the whole board, including the target, when the STLink sucessfully enumerates (or if this is overriden using the JP2 jumper).
Note, that 3V_OUT is shorted to 3V3.
JW
2020-05-25 3:43 AM
PWR_ENn enables power to the whole board, including the target, when the STLink sucessfully enumerates (or if this is overriden using the JP2 jumper).
Note, that 3V_OUT is shorted to 3V3.
JW
2020-05-25 3:45 AM
Oh I see. Thanks, that makes sense