cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L053 Standard Peripheral Library

alfred
Associate
Posted on April 24, 2014 at 11:34

Hi All,

I am designing the Heat Meter with STM32L053 now.

So have you released STM32L053 Standard Peripheral Library yet please?

It is very important to speed up our design schedule.

Thanks.

#stm32l053
6 REPLIES 6
mhessler9
Associate
Posted on April 28, 2014 at 10:12

Hi Community,

I'm also interested in using the standard peripherals library for the STM32L0.

Thanks!

SeaFood
Associate II
Posted on April 28, 2014 at 17:48

There will be 2 firmware options for STM32L0:

  • STM32CubeL0:

    http://www.st.com/stm32cube

     initiative ported onto STM32L0, solution to easily switch from one STM32 to another: high portability solution - Availability for... this week !
  • STM32SnippetsL0: STM32Snippets initiative, as done on

    http://www.st.com/stm32snippets

    , collection of examples directly based on registers: high optimization solution - Availability for end of June 2014

Posted on April 28, 2014 at 19:11

Yeah, that's great and all, but I'd also like to see the firmware library ported.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on June 25, 2014 at 10:11

A few days ago the ST released STM32L0 Snippets at:

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1898/PF260788#

but when you click at the bottom of the page to get the software you will download the Cube L0 instead (the name of the package is stm32snippetsl0.zip but the actual content is Cube L0)

Weird, as I expected the Snippets, NOT Cube L0.
jephua
Associate II
Posted on September 30, 2014 at 04:58

I am also interested in the standard peripheral library for STM32L053, any updates whether it will be available?

anna23
Associate II
Posted on October 08, 2015 at 10:36

Hi, I am looking for that library too... Where I can get it?

Thanks