cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H755 Supply connection

koyocik
Associate II

Hello,

I'm working on project with STM32H755ZIT6. Currently I use Nucleo Board, but I designed prototype board, but the board don't work. I supose that problem is caused by wrong connection for supply.

I use +3.3V from DC/DC connerter for suplly. Can someone help to find out where could be the problem?

Thank you all in advance for any tips.

1 ACCEPTED SOLUTION

Accepted Solutions

Because from the beginning you configured the MCU with the wrong power config.

You need to recover your board from that situation and set the correct power supply SMPS or LDO. Read this article:

https://community.st.com/t5/stm32-mcus/how-can-i-recover-my-stm32h7-board-after-facing-a-power/ta-p/49579

For the schematics, I invite you again to look at the schematics of NUCLEO-H753ZI for LDO: https://www.st.com/resource/en/schematic_pack/mb1364-h753zi-c01_schematic.pdf

and NUCLEO-H753ZI for SMPS: https://www.st.com/resource/en/schematic_pack/mb1363-h755ziq-d01_schematic.pdf

PS: you don't need to set VOS level in two steps.  Keep VOS0:

	__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
	
	while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

And remove the settings of VOS1.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

13 REPLIES 13
mƎALLEm
ST Employee

Hello,

Need to check first your power supply config in the application versus what do you have on the HW.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hello,

 

Please check below:

void SystemClock_Config (void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

    /** Supply configuration update enable
    */
    HAL_PWREx_ConfigSupply(PWR_DIRECT_SMPS_SUPPLY);
    /** Configure the main internal regulator output voltage
    */
    __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);

    while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
    /* Initializes the RCC Oscillators according to the specified parameters
    * in the RCC_OscInitTypeDef structure. */

  /* Configure LSE Drive Capability  */
  HAL_PWR_EnableBkUpAccess();
  __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);

  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;
  RCC_OscInitStruct.HSEState = RCC_HSE_ON;
  RCC_OscInitStruct.LSEState = RCC_LSE_ON;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
  RCC_OscInitStruct.PLL.PLLM = 5;
  RCC_OscInitStruct.PLL.PLLN = 192;
  RCC_OscInitStruct.PLL.PLLP = 2;
  RCC_OscInitStruct.PLL.PLLQ = 2;
  RCC_OscInitStruct.PLL.PLLR = 2;
  RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_2;
  RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
  RCC_OscInitStruct.PLL.PLLFRACN = 0;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
                              |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
  RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
  RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
  {
    Error_Handler();
  }
}

 

From your side please review your schematics and check if there is somethong wrong with SMPS HW by comparing it to NUCLEO-H755ZI schematics: https://www.st.com/resource/en/schematic_pack/mb1363-h755ziq-d01_schematic.pdf

And according to your code you are setting the SMPS and this configuration you cannot exceed 400MHz at VOS1.

From the datasheet:

SofLit_0-1730551843862.png

 

 

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thank you for your answer.

I created my schematic based on nucleo schematic, but I'm not sure if it is correct, because as I said before the prototype board doesn't work.

Do you have any example which show how configure software to run with maximal clock 480MHz?

For internal SMPS, the capacitors on VCAP should be pair of 100nF not 2u2F ?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

@koyocik wrote:

Do you have any example which show how configure software to run with maximal clock 480MHz?


In SMPS configuration you can't reach that frequency. That's what I'm saying. 

To reach 480MHz you need to be in LDO mode and your hardware needs to follow. Example: NUCLEO-H753 which is set in LDO config by HW.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thank you for answer. Sumarize I should do as following:

1. Connect hardware same way as STM32H753 (see attachment).

2. Change software part as following:

void SystemClock_Config (void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  /*!< Supply configuration update enable */
  HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);

  /* The voltage scaling allows optimizing the power consumption when the device is
     clocked below the maximum system frequency, to update the voltage scaling value
     regarding system frequency refer to product datasheet.  */
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

  while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

  /* Configure LSE Drive Capability  */
  HAL_PWR_EnableBkUpAccess();
  __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);

  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;
  RCC_OscInitStruct.HSEState = RCC_HSE_ON;
  RCC_OscInitStruct.LSEState = RCC_LSE_ON;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
  RCC_OscInitStruct.PLL.PLLM = 5;
  RCC_OscInitStruct.PLL.PLLN = 192;
  RCC_OscInitStruct.PLL.PLLP = 2;
  RCC_OscInitStruct.PLL.PLLQ = 2;
  RCC_OscInitStruct.PLL.PLLR = 2;
  RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_2;
  RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
  RCC_OscInitStruct.PLL.PLLFRACN = 0;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
                              |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
  RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
  RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
  {
    Error_Handler();
  }
}

 

How should I connect pins 15 (VDDSD), 16 (VLXSD), 17 (VFBSD)?

Hello,

This is how to connect SMPS  pins when you are in LDO mode:

From Figure 22 / RM0399:

SofLit_0-1730716354435.png

VDDSMPS: Connect to GND.
VLXSMPS: Leave unconnected (NC).
VFBSMPS: Connect to GND.
VSSSMPS: Connect to GND.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thank you for answer on that. I try wire my prototype board somehow to get this connection.