cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H753VIH6 RMII

Manikandan
Associate II

Hi Team,

 

We are using the STM32H753VIH6 in our design.

 

We are connecting the Realtek RTL8364 through RMII interface.

Connections are in the attachment and we have validated link between the two.

I have captured the waveforms , but the voltage span looks incorrect(going beyond 3.3V)  because the STM is powered by 3.3V.

 

Need inputs to capture proper waveforms.

 

Thanks

Manikandan R

5 REPLIES 5
STOne-32
ST Employee

Dear @Manikandan ,

 

Looking to the waveforms, there is a serious issue with signal integrity !  can you please share your schematics and lines RMII Terminations ? including the Clock of 50MHz and how is generated.  So, Our valuable community members  can help further.

 

STOne32_0-1742369612599.png

Ciao

STOne-32.

 

Manikandan
Associate II

Hi

 

The STM32 and Realtek RTL8364 are connected with 0E resistor in series.

 

 

Manikandan_1-1742377038863.png

 

Manikandan
Associate II

Dear ST community,

Any inputs on the Voltage span of the signals will be much appreciated.

 

Thanks

Manikandan R

Hello,

I think better to inspire from one of the ref designs of ST boards:

From Nucleo-H743 schematics:

mALLEm_0-1742377523329.png

From STM32H743-Eval schematics:

mALLEm_1-1742377556371.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Manikandan
Associate II

Dear ST community,

Is the external PU is mandatory?

As per this reference let me introduce 33E in the series path of CLK, RXD0,RXd1,CRS_DV and will capture the waveforms.

Any inputs on the Voltage span ?

Thanks 

Manikandan R