cancel
Showing results for 
Search instead for 
Did you mean: 

stm32H750VBT6 CAN bootloader

Dllamas21
Associate II

Hello,

I am trying to confirm that there is not CAN boot loader for the STM32H750VBT6 LQPF100/144 packages. Attached is the pin out included PH13 and PHY 14 and snipped form AN2606 for the STM32H75xx.

 

Thanks!

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Dllamas21 

I can confirm that there is no FDCAN bootloader since it is available only for FDCAN1 on PH13 and PH14 that are not available on the LQFP100 and LQFP144 Packages of the STM32H750VB. But you still can use the open bootloader.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @Dllamas21 

I can confirm that there is no FDCAN bootloader since it is available only for FDCAN1 on PH13 and PH14 that are not available on the LQFP100 and LQFP144 Packages of the STM32H750VB. But you still can use the open bootloader.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Dllamas21
Associate II

Thanks!