Skip to main content
Associate
October 7, 2024
Question

STM32F0 bootloader

  • October 7, 2024
  • 10 replies
  • 2886 views

Dear Members,

I'm using the STM32F030CC controller for my RTOS-based project and currently developing a bootloader for it. The application code has been relocated to 0x08004000. The bootloader successfully jumps to the application, but after initializing all peripherals (GPIO, timers, etc.), calling `HAL_GetTick()` returns a `uwTick` value of 0.

Sid_sid_2-1728297669622.png

This is the fuction iam using to jump from bootloader to application. when i try to do _enable_irq(); the jump fuction is not working . 

am i missing anything?

This topic has been closed for replies.

10 replies

Andrew Neil
Super User
October 7, 2024

Please see the Posting Tips for how to properly post source code - not as an image:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Technical Moderator
October 7, 2024

Hello @Sid_sid and welcome to the community,

First, please use </> button to paste your code instead of sharing screen shots.

Second, Did you remap your vector table (VTOR) to the new Flash address 0x08004000?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Sid_sidAuthor
Associate
October 7, 2024

Thankyou for your reply.

are you asking about the linker script in application?

* Specify the memory areas */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 32K
FLASH (rx) : ORIGIN = 0x08004000, LENGTH = 240K
}
mƎALLEm
ST Technical Moderator
October 7, 2024
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
TDK
October 7, 2024

You are disabling interrupts which prevents systick from occurring.

 

For working code on how to jump to the bootloader, see here: It can be easily modified to jump instead to your application. Note the section where it disables interrupts in the NVIC registers. You likely need something similar

How to jump to system bootloader from application ... - STMicroelectronics Community

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
October 7, 2024

Calling from an Interrupt Handler (say EXTI or whatever) can be problematic due to how the NVIC unwinds priority. See also callback's operating from interrupt context.

RTOS can be problematic from a System / User context type point of view

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Sid_sidAuthor
Associate
October 8, 2024

when i try __enable_irq(); in application, the code stuck there.

But when i tried a basic led blink project as an application code ,that was worked and the uwTick is icrementing.

This is the bootloader jump function.

void Bootloader_JumpToApplication(uint32_t address)
{

 
 // disable global interrupt
 __disable_irq();

 // Disable all peripheral interrupts
 HAL_NVIC_DisableIRQ(SysTick_IRQn);

 // main app start address defined in linker file
 extern uint32_t _main_app_start_address; 

 uint32_t MemoryAddr = (uint32_t)&_main_app_start_address;
 uint32_t *pMem = (uint32_t *)MemoryAddr;

 // First address is the stack pointer initial value
 __set_MSP(*pMem); // Set stack pointer

 // Now get main app entry point address
 pMem++;
 void (*pMainApp)(void) = (void (*)(void))(*pMem);

 // Jump to main application (0x0800 0004)
 pMainApp();
 
}

 this is the starting of application code:

int main(void)
{
 /* USER CODE BEGIN 1 */
 // Copy interrupt vector table to the RAM.
 volatile uint32_t *VectorTable = (volatile uint32_t *)0x20000000;
 uint32_t ui32_VectorIndex = 0;

 for(ui32_VectorIndex = 0; ui32_VectorIndex < 48; ui32_VectorIndex++)
 {
 VectorTable[ui32_VectorIndex] = *(__IO uint32_t*)((uint32_t)FIRMWARE_START_ADDR + (ui32_VectorIndex << 2));
 }

 __HAL_RCC_AHB_FORCE_RESET();

 // Enable SYSCFG peripheral clock
 __HAL_RCC_SYSCFG_CLK_ENABLE();

 __HAL_RCC_AHB_RELEASE_RESET();

 // Remap RAM into 0x0000 0000
 __HAL_SYSCFG_REMAPMEMORY_SRAM();

 // __enable_irq();
 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_USART1_UART_Init();
 MX_TIM17_Init();
 MX_ADC_Init();
 MX_I2C1_Init();
 MX_TIM15_Init();
 MX_USART5_UART_Init();
 MX_CRC_Init();
 MX_USART3_UART_Init();
 MX_RTC_Init();
 MX_USART4_UART_Init();

 

TDK
October 8, 2024

> when i try __enable_irq(); in application, the code stuck there.

Probably because you did not disable interrupts correctly.

"If you feel a post has answered your question, please click ""Accept as Solution""."