cancel
Showing results for 
Search instead for 
Did you mean: 

stm32h750vbt6 adc 16bit 14bit issue

mize
Associate III

Hello,

mize_0-1723793714498.png

while using this mcu 16bit adc a strange thing happens.

the adc signal is test under a sinusoid signal(0.5Hz from a signal generator), and as shown in the figure at certain level adc keeps unchanged, after leaving this level then the signal increased again, however the trace has deviate from a standard sin signal.

as I checked the value is 0d57345 which is 0b1101 1111 1111 1111 and this phenomenen occurs everytime the 14th bits is 0 and lower bits are 1.(at 0b0001 1111 1111 1111, 0b0101 1111 1111 1111, 0b1001 1111 1111 1111 a value constant platform occurs)

mize_1-1723793728792.png

and at some other points there is a leap where the trace goes back to original trace.

mize_2-1723794431864.png

this happens for 14bits resolution adc sometimes as well.

mize_3-1723794529822.png

sometimes for 15th bit as well.

I have tried several times to fix this including

1.longer sampling cycs

2.longer delay between conversion

3.independent mode/ dual mode(adc1, adc2)

4.LL LIB/HAL LIB

5.fast/slow adc clock

6.calibration/no calibration before enable and start conversion

7.fast/slow channel

none of above worked, so anyone have any idea please kindly reply

thanks

 

IOC file has been attached and my cube version is 6.12.0-RC9

 

 

13 REPLIES 13
TDK
Guru

Generally, this is caused by a poorly decoupled VDDA or VREF+ supply. Can you share your schematic/layout?

If you feel a post has answered your question, please click "Accept as Solution".
STOne-32
ST Employee

Dear @mize ,

 

if possible to share your hardware schematics : the exact MCU part number and package ,decoupling and which channels used . Here is an App Note on this 16-bits ADC and its performance. The input signal is also key to be very clean from a low noise source - using a standard lab generator and wires hooks at 16-bits should be carefully designed.

https://www.st.com/resource/en/application_note/an5354-getting-started-with-the-stm32h7-series-mcu-16bit-adc-stmicroelectronics.pdf

Hope it helps ,

STOne-32

mize
Associate III

mize_0-1724028711438.png

mize_2-1724028725098.png

mize_3-1724028750325.png

 

Hi, this is my schematic diffierential signal pair from sensor amplified by ina8211dr then directly feed to MCU ADC channel.

There is one problem that I have disscussed with my hardware colleague that the capacitor between VDDA/GND and Vref+/GND is different with the AN2834 recommanded schematic that bypass capacitor with 1uf//1nf 1uf//100uf, but he says it won't affect too much, I'm not so sure about this for I mainly doing software, what's your opinion? 

mize_4-1724029715202.png

 

mize
Associate III

mize_0-1724035691627.png

and Vref+ is indenpent with VDDA

Hi,

  I have shared my relevant schematics in other replies, please refer to it. I tried two source, one was from designed sensor and amplified and one was directed from a signal generator device. So it is mostly a MCU problem, the chip I'm using is STM32H750VBT6 V 7837C VQ PHL 78 335  with QFP100 package, the VDDA and Vref+ are independently from different LDO and at different level. 

 I have tried fast channel 4,5 slow channel 7,8, and another MCU for I have 2 sample.

 

And as I have mentioned in other reply: There is one problem that I have disscussed with my hardware colleague that the capacitor between VDDA/GND and Vref+/GND is different with the AN2834 recommanded schematic that bypass capacitor with 1uf//1nf 1uf//100uf, but he says it won't affect too much.

mize_1-1724036717451.png

So if you have any further idea please kindly comments, thanks a lot!

 

How are A_3.3V and ADVREF being generated?

A 1 uF cap can help things. Since you are seeing issues, and this issue can be cause by improper decoupling caps, I would suggest fixing that in hardware to see if it makes a difference. It is the most logical thing to check first.

GND and AGND should be tied directly, or (perhaps better) not be separate at all. Presumably they are, but not that 0 Ohm jumper resistor are not really 0 ohms.

Everything else seems okay. I'm assuming there are decoupling caps on each power pin, but that's not likely to be the cause here even if it's not true.

If you feel a post has answered your question, please click "Accept as Solution".

From my experience with nucleo-H743zi2 board (stm32H743zi2) - all decoupling capacitors circuits designed by ST, and board manufactured by ST, ADC bits 12-13-14-15 are just noise. Doesn't matter how low source impedance of the inputs driver or what reference voltage is. IC package could be a cause.

 The only way to get 16-bits is using oversampling, running adc as fast as possible.

BTW, ad821 is powered by 5V may presents risk of damaging IC, consider 3.3V powered buffer for that. LM358 for reference is also wrong choice, OPA  has not sufficient GBW to drive switching capacitive load. In both sides - reference inputs and signal inputs good capacitance required to null out charge kickback interference. Look on google for correct SAR adc interfacing.

mize
Associate III

HI TDK,

 I tired fix the 1uf cap today but not work. 

 power supply are generated from LDOs, which is adaptor 12v-> LM1117MPX 5v -> TPS73633DBVR 3.3v -> TL431AIDBZR ADVREF. AGND/GND are tighted through a 0ohm, perhaps I should remove it. But it seems not where problem lies.

guess I need to give up internal adc, thx any way.

mize
Associate III

HI,

@MasterT  @TDK  @STOne-32 

I have a hypothsis. The possible cause is that there is a voltage drop of 2-3mV (according to collected data presumably, something equavilent to the diode/transistor drive threshold voltage)  exists when comparing the 14th bit, and does not exist when comparing other bits,  thus causing the input voltage to comparator for bits 14 is lower than it should be.

 

mize_1-1730430309186.png

STM32's SAR working flow is by charging the capacitor, reversing the input voltage to ground, and controlling different switches to obtain different voltage dividers to make the input voltage equal to -Vin+Vref voltage dividers, and then comparing the value of 0 with the comparator to obtain the ADC code.

here is some deduction, suppose the actual input voltage is V, and the drop value is Vd

  1. for level flat phase, in the 14th bit of comparison, the external input voltage is V, but the input comparator voltage is V-Vd, where V14<V<V14-Vd, so the output value of V 14th bit is always 0.
    This voltage drop persists in successive phases after the levelling phase, and the actual input comparator voltage is V-Vd, so there is a fixed bias compared to the real voltage.(like in first figure)
  2. after that, when V15 < V, the input voltage to the comparator is V when comparing V15, and 15th bit is encoding to 1, causing the voltage to leap directly from V-Vd to V( like in second figure)
  3. until the next time, when  V14 <V-V15 <V14-Vd, the situation comes back at level flat phase, that happened again
  4. For example, 32768 (1000 0000 0000 0000) is a number that can be successfully read, at this time it should be S1 connected to VREF, and other switches are connected to ground. The next time evel flat happens again, it is 40959 (1001 1111 1111 1111 1111), and the problem is 14th bit, and when comparing the 14th position, it is S1(bit16), S2(bit15), and S3(bit14) connected to Vref, so the guess here is that S3(bit14) makes a voltage drop when it connected to VREF, and this is the only situation where voltage drop exists, so that the input voltage is less than the actual voltage, resulting in the abnormality of the ADC

 

however it is impossible for me to check the design inside MCU (like the e-switch type is in use) , so this only will be a theory. I have attached a data record for reference. enjoy&thx