cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H750 RAM configuration

etamarin
Associate III

I am looking into RAM support for the SMT32H750 series chips for my future projects.

The STM32H750 series chips support 16-bit data bus as well as 32-bit data bus configuration. This mode is selected on startup, as far as I can tell.

If I were to use the STM32CubeMX tool to configure my chip, would a switch from a 16 bit to a 32-bit bus (and vice versa) require a significant re-generation of support code, or would it be realtively easy to toggle this (ignoring the pin reassignments)?

I would test this myself but it seems like all development kits for this series have a 16-bit data bus...

1 ACCEPTED SOLUTION

Accepted Solutions

It should be relatively localized, probably mostly in the MSP code, and the initialization of the pins,and the FMC / SDRAM

Whether those new pins displace prior usages, and how disruptive that is to hard coded usage in other parts of the code will determine how complex the refactoring will be. Hard to call from here, but shouldn't be intractable..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

7 REPLIES 7

Internally it's 32-bits

Externally it's going to depend on how the FMC is configured, the package size vs pin availability and connectivity to the SDRAM, etc. From lower pin count devices 16 bits wide might be the most practical trade off, especially if RGB TFT LCD is also used and consuming pins.

If that's not what you mean you're going to need to be more specific.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

I have enough pins to satisfy both a 32 and a 16 bit bus. However I am also working with software derived from a legacy design that used a 16-bit chip (long story). So I am wondering if I will have to do a lot of refactoring if I switch to 32-bit mode, or if this can be a "painless" procedure.

Hello @etamarin 

The extent of this refactoring would depend on how closely your software interacts with the hardware. If it's mostly high-level code, the impact could be minimal. But if it's low-level code that directly manipulates hardware registers, more extensive changes might be needed.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


TDK
Guru

It takes very little code, all contained within the initialization, to change between 16 and 32-bit FMC bus.

If you feel a post has answered your question, please click "Accept as Solution".

It should be relatively localized, probably mostly in the MSP code, and the initialization of the pins,and the FMC / SDRAM

Whether those new pins displace prior usages, and how disruptive that is to hard coded usage in other parts of the code will determine how complex the refactoring will be. Hard to call from here, but shouldn't be intractable..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
etamarin
Associate III

Thanks all for the inputs. Looks like I might pull it off :)

I was also thinking to test it on some kind of evaluation board, but can't find one with a wide bus. Is something like this available for purchase?

Hello,

For 16-bit SDRAM you can use STM32H750 discovery board.

For 32-bit SDRAM you can use STM32H743 Eval board but it's more expensive.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.