cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H750 issue switching system clock to PLL1

_MaticBabnik
Associate

I'm trying to get the STM32H750 discovery board running at 400MHz with as little code as possible. (plain C with ST's startup file, cherry-picking structs and defines from CMSIS)
As far as I can tell I do most of the things, ST's examples do before and in SystemClock_Config.
Using a debugger I checked the following registers just before switching the clock source to PLL1.

 

Register    | ST's example | difference?

RCC
	CR			0303 7025   . 
	CIER		 		0	.
	CFGR		 		0	.
	D1CFGR		       48	.
	D2CFGR		      440	.
	D3CFGR		       40	.
	PLLCKSELR	 202 0052	dont have DIVM2 AND DIVM3;
	PLLCFGR		 1ff 0009	dont have PLL2,3 cfg
	PLL1DIVR	 103 029f	.
	PLL1FRACR	 		0	.
	AHB2ENR				0	.	
	AHB3ENR				0	.
	AHB4ENR		        0 	.	
	APB4ENR		   1 0002	.
SCB
	SHCSR				0	.
	CCR		   	   7 0210	no caches
PWR
	CR3		     500 0042	.
	D3CR		     e000 	.
	CSR1		     e000	.
SYSCFG
	CCCSR			    0	.
FLASH
	ACR		           37   .

 

 After the switch my code gets stuck waiting for PLL1 in SWS.
Any ideas why the clock doesn't switch? Could the lack of PLL2,3 config be the reason?

1 REPLY 1
AScha.3
Chief III

Why don't you use Cube / HAL, set clock tree and debug etc, generate code and then just look, how it's done. If you can do same better, then you still can try . But have a reference, how exactly your configuration can be initialized.

If you feel a post has answered your question, please click "Accept as Solution".