cancel
Showing results for 
Search instead for 
Did you mean: 

STM32h745iik6 doesn't execute code on power up, execution starts after i press reset manually

dplogiic
Associate II

Hello everyone,

I'm experiencing an issue with my STM32 microcontroller (STM32h745iik6 own board) where it doesn't execute the code upon power up. However, when I press the reset button, the code executes as expected. I'm looking for some guidance to resolve this problem.

bellow i attach some schematic. please suggest how can i solve this challenges.

dplogiic_0-1718799088435.pngdplogiic_1-1718799114713.pngdplogiic_2-1718799141128.pngdplogiic_3-1718799182847.pngdplogiic_4-1718799263776.png

dplogiic_5-1718799283302.png

 

10 REPLIES 10
Peter BENSCH
ST Employee

Please place a capacitor of approx. 100nF between NRST and GND.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
SofLit
ST Employee

You need to check VCAP capacitors. Did you mount them? how much?

You need also to provide the complete schematics (mostly the MCU part) to help you efficiently.

Also need to place a capacitor on NRST/GND as stated by my colleague @Peter BENSCH 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

hello @Peter BENSCH @SofLit ,

I trying to 1) place 100nF/25v cap near nsrt 

2) i try to disconnect all and only place 100nF cap with GND like below 

dplogiic_0-1718866821767.png

but even not work.

3) if i disconnect reset ckt  so nsrt pin present 3.263v.. and just i touch any cable to nsrt then controller reset and code execute well.. ......

dplogiic_1-1718867125424.png

So actually what is issue.. any pull up/ pull dawn needed to add externally.

4) on Boot0 pin connection like below  

add 1uf/25v cap to Boot0 with 3.3v and 10k gnd

dplogiic_2-1718867441603.png

my board upload program by external stlinkv3 programmer...  if i remove 1uF cap of boot0 then error while upload code...    but if i connect like above then program upload successfully... and debug also.. but i remove stlink then code not execute until i press nsrt every power up. 

Peter BENSCH
ST Employee

It is definitely wrong to place a capacitor from BOOT0 to VDD. Similarly, no pull-up is necessary at NRST, even if it is incorrectly shown in some colourful "Pills".

@SofLit  has pointed out that the corresponding capacitors must also be connected to the VCAP pins. For your STM32H745IIK6 in the UFBGA176+25, these are A4, A14 and R13. Have you done this?

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Vcap A4, A14, R13 connected with 2*2.2uF/50v---> GND

Peter BENSCH
ST Employee

With the current information, this is difficult to assess. It could be a layout problem, one with the solder joints of your UFBGA, and so on.

If you touch the open NRST pin with your finger, you only inject noise, which trigger the same thing as a short low pulse.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

As I already suggested, you need to share your schematics. We don't have the full picture here so we cannot help you efficiently. Also share your ioc file to check the init.

You can also refer to the AN4938 "Getting started with STM32H74xI/G and STM32H75xI/G
MCU hardware development" and also to our reference design stm32h745i-disco schematics.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.
dplogiic
Associate II

Hello @SofLit @Peter BENSCH ,

I want code run by default when power on. Now it detect usb dfu boot mode by default. and i'm able to upload code using usb dfu without touching boot pin. but all time i need to manually press reset button for going in user_application mode. means i power on the board i need to press reset then code run. bcoz it going in usb dfu mode by default when power on.     

dplogiic_7-1722833571747.png

 

I attach schematic file below for your reference. Please suggest my what I'm wrong. 

I refer the schematic file of board Nucleo-H745ziq NUCLEO-H745ZI-Q - STM32 Nucleo-144 development board with STM32H745ZI MCU, SMPS, supports Arduino, ST Zio and morpho connectivity - STMicroelectronics

dplogiic_0-1722831728311.png

dplogiic_1-1722831754384.png

For supply configuration i'm using below,

dplogiic_6-1722833112665.png

 

 

 

 

 

Check there are proper vectors at 0x08000000

Instrument Error_Handler and HardFault_Handler so that you might know if it ends up in either of those to die silently. 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..