2022-11-01 10:48 AM
Hi I have been trying to change the read protection level on my device using the ST HAL driver library:
The code I am using is:
FLASH_OBProgramInitTypeDef OB_Config;
//Read Option byte configuration
HAL_FLASHEx_OBGetConfig(&OB_Config);
//Update read protection option byte
OB_Config.OptionType = OPTIONBYTE_RDP;
OB_Config.RDPLevel = OB_RDP;
//Program new option byte configuration
bool option_bytes_failed_to_update{true};
if(HAL_FLASH_OB_Unlock() == HAL_OK)
{
if(HAL_FLASH_Unlock() == HAL_OK)
{
if(HAL_FLASHEx_OBProgram(&OB_Config) == HAL_OK)
{
if(HAL_FLASH_OB_Launch() == HAL_OK)
{
if(HAL_FLASH_OB_Lock() == HAL_OK)
{
if(HAL_FLASH_Lock() == HAL_OK)
{
option_bytes_failed_to_update = false;
}
}
}
}
}
}
When the function HAL_FLASH_OB_Launch() is makes a call to status = FLASH_OB_WaitForLastOperation((uint32_t)FLASH_TIMEOUT_VALUE); which causes a hard fault.
Has anyone had a similar experience with this device and possibly a pointer to what I am doing wrong?
2022-11-25 6:42 AM
Hello @ILave.1,
If debugger access is detected then R/W/Erase to FLASH memory, SRAM, and Backup registers are blocked (hard fault generated).
So, I suggest the following sequence
You can check this MOOC and its attached resources
STM32 Security tips - 4 RDP without POR in STM32F4 - YouTube
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.