2022-10-14 05:46 AM
I downloaded the software pack from Github STM32CubeH7/Projects/STM32H745I-DISCO/
, and followed the instructions in UM2222 manual.
I can connect st link com port. But no data is shown on the oscilloscope window.
2022-10-14 06:51 AM
Hello @DZhan.9 ,
Did you follow the instruction in the readme file ?
Make sure to Apply an external signal to the board input (PA0, CN7 Connector pin A2).
Imen
2022-10-14 07:19 AM
Yes. I connected it to the DAC output. I verified the DAC output using my own scope. It works as expected.
I also tried Wireshark to check USB communication. I cant see packets between the microcontroller and my laptop.