cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743ZI Direct channels for ADC.

GHARI.1
Associate II

Hi,

I am using STM32H743ZI micro controller of LQFP144 package. My doubt is that in the data sheet they are mentioning that it has 2 direct channels for ADC but they are not mentioning what are the channels or pins offering this

They are only talking about TFBGA240 +25 package pins offering this direct concept then what about LQFP-144 pins offering this.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
MM..1
Chief III

. Direct channels are connected to analog I/Os (PA0_C, PA1_C, PC2_C and PC3_C) to optimize ADC performance

View solution in original post

1 REPLY 1
MM..1
Chief III

. Direct channels are connected to analog I/Os (PA0_C, PA1_C, PC2_C and PC3_C) to optimize ADC performance