cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743VIT6 vs STM32H743ZIT6

eLKa
Associate II

Hello everyone.

Is it possible to directly replace STM32H743VIT6 processor with STM32H743ZIT6 without changing the program code? Will there be any differences in the performance of the DSP device with this processor?

Thanks in advance for your reply, Chris.

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,

It depends on how do you mean by direct replacement.

STM32H743VIT6 is 100 pin package while STM32H743ZIT6 is 144 pin package. So the only difference is the pin number / IOs:

Please refer to the datasheet Table 2 where the features of each part number are provided:

SofLit_0-1712651227396.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

5 REPLIES 5
SofLit
ST Employee

Hello,

It depends on how do you mean by direct replacement.

STM32H743VIT6 is 100 pin package while STM32H743ZIT6 is 144 pin package. So the only difference is the pin number / IOs:

Please refer to the datasheet Table 2 where the features of each part number are provided:

SofLit_0-1712651227396.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Thank you very much for your quick reply. I was mainly concerned with changes in the program code.

Apart of the PCB  footprint, the two part numbers have the same die. So you can replace STM32H743VIT6 by STM32H743ZIT6 without any issue.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

The datasheet also tells you what all those suffix characters mean in the part number:

AndrewNeil_0-1712656039200.png

 

eLKa
Associate II

Thank you all for your answers. It helped me a lot. All you need to do is redesign the printed circuit board.