2026-01-24 12:46 AM - last edited on 2026-01-26 12:23 AM by mƎALLEm
Hello all
Hardware
stm32h743iitx
flash : W25Q256JV
sdRam: w9825g6kh
lcd : 7 pouces no driver 24bit parrallel
I have dev a stm32h743ii pcb with a 7 pouces 24 bit lcd . the basic debug work for the lcd and sdram
Where i am facing problem is on flash W25Q256JV qspi work fine just with 1 line but impossible to make working bank 1 with 4 lines.
Can i have some confirmation with the community about :
if someone has experiment something please share i going crasy ........
2026-01-26 12:38 AM
Hello @KNaim.1;
What do you mean by "impossible to make working bank 1 with 4 lines."?
Is it possible to read the device ID?
Are you having problems reading or writing?
Can you share the command instructions configuration?
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.