cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743 system bootloader cannot program flash by I2C

It is not a question but info for others.

STM32flash app on RPi can connect to STM32H743 on NUCLEO board (tested on SPI2).

AN2606 says "Bank erase is not working on USART/SPI and I2C" but even page-by-page erase does not work so CPU cannot be programmed.

STM32flash does not show the bootloader version but the NUCLEO was purchased at the end of 2019.

Reading of flash memory works.

1 REPLY 1
haleecaero.1
Associate II

> STM32flash app on RPi can connect to STM32H743 on NUCLEO board (tested on SPI2).

@Community member​ could you share a link to a version of stm32flash which supports SPI ? I cannot find it

thanks