cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f373r8t6 - CAN not working at 1Mbit / s

Nikolai_Werenich
Associate

Hello forum users!

Created a project by example

[url] https://istarik.ru/blog/stm32/159.html [/ url]

Slightly corrected, so that a new frame is sent every 10 msec.

The project works at (except one) any speed (100kbit - works, 500, 800 - works).

Data is transmitted and received by a usb-can converter (sys tec elecronic).

Here, for example, I configured the project for a CAN speed of 500kbit / s:

- here is the CAN tincture:

[url = http: //vfl.ru/fotos/6049ccb837010333.html] [img] http://images.vfl.ru/ii/1638964027/6049ccb8/37010333_m.jpg [/ img] [/ url]

- and here is the frequency setting:

[url = http: //vfl.ru/fotos/d34be44637010398.html] [img] http://images.vfl.ru/ii/1638964156/d34be446/37010398_m.jpg [/ img] [/ url]

-and this data is received at a speed of 500 kbps:

[url = http: //vfl.ru/fotos/2ec1947737010697.html] [img] http://images.vfl.ru/ii/1638965166/2ec19477/37010697_m.jpg [/ img] [/ url]

- this is the picture on the CAN bus:

[url = http: //vfl.ru/fotos/d52d156337010759.html] [img] http://images.vfl.ru/ii/1638965437/d52d1563/37010759_m.jpg [/ img] [/ url]

************************************************* *********

Okay, reconfiguring the speed to 1Mbps.

To do this, you just need to change the CAN frequency divider from 4 to 2.

And Cube kindly calculates the bus speed:

[url = http: //vfl.ru/fotos/75dbe36237010531.html] [img] http://images.vfl.ru/ii/1638964501/75dbe362/37010531_m.jpg [/ img] [/ url]

I'm flashing the microcontroller and that's it. Data is not accepted :(, but on the bus this is the picture:

- to fit everything into the monitor, I had to change the sweep to 100msec !!!!

[url = http: //vfl.ru/fotos/b265ca8237010856.html] [img] http://images.vfl.ru/ii/1638965896/b265ca82/37010856_m.jpg [/ img] [/ url]

At the same time, if you look at the status of the registers, then CAN reports and sets error bits:

[url = http: //vfl.ru/fotos/75f6ccfa37010945.html] [img] http://images.vfl.ru/ii/1638966181/75f6ccfa/37010945_m.jpg [/ img] [/ url]

LEC Bits in ESR Register: 101: Bit dominant Error

Why does stm32 not want to work at a CAN speed of 1 Mbit / s ???

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
mƎALLEm
ST Employee

Hello @Nikolai_Werenich​ ,

Could you please increase the system clock to 72MHz (AHB prescaler = 1, APB1 prescaler = 2)?

Also for the sample point it's recommended to set it at about 88% of the bit time at higher bitrates.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.