cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743 RTC Clock configuration failure

anilgayakwad
Associate

Hello, 

I'm working on STM32H743BIT6, It is in production phase. During flashing the software, it is failed to configure LSE crystal with internal RTC enabled. out of 50 boards 2 board got failed.

During debug it is observed that the RTC clock configuration is getting failed.

Kindly support us for resolving the issue

 

Thank You

Anil Gayakwad

1 REPLY 1
mƎALLEm
ST Employee

Hello,

Not sure what do you mean by "During flashing the software, it is failed to configure LSE crystal with internal RTC enabled". ?

Do you mean that the RTC failed to be configured at your application startup? and what is the symptom? enable to write to a register or what?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.