2018-04-07 6:15 AM
Hi all,
To start with:
Board: STM32H743ZI Nucleo
IDE: Attolic TrueSTUDIO for STM32 9.0.0
HAL version: STM32Cube_FW_H7_V1.2.0
I'm trying to trigger a DMA transfer on DMA1_Stream7 using TIMER 3 CC3. I want to trigger a transfer from a variable into the CCR for TIM3 channel 3.
I can initial the DMA stream to the configuration I think it should be in but as soon as the stream is enabled I get a transfer error and I can't work out what the problem is.
Any help would be great.
Thanks
Below is a screenshot of DMA1, stream 7 register values.
Below is my DMA stream initialisation code:
void setUpDMA(TIM_HandleTypeDef *htim)
{static DMA_HandleTypeDef hdma_tim;
/* Enable DMA clock */
__HAL_RCC_DMA1_CLK_ENABLE();/* Set the parameters to be configured */
hdma_tim.Init.Request = DMA_REQUEST_TIM3_CH3; hdma_tim.Init.Direction = DMA_MEMORY_TO_PERIPH; hdma_tim.Init.PeriphInc = DMA_PINC_DISABLE; hdma_tim.Init.MemInc = DMA_MINC_DISABLE; hdma_tim.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD; hdma_tim.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD; hdma_tim.Init.Mode = DMA_CIRCULAR; hdma_tim.Init.Priority = DMA_PRIORITY_HIGH; hdma_tim.Init.FIFOMode = DMA_FIFOMODE_DISABLE; hdma_tim.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL; hdma_tim.Init.MemBurst = DMA_MBURST_SINGLE; hdma_tim.Init.PeriphBurst = DMA_PBURST_SINGLE;/* Set hdma_tim instance */
hdma_tim.Instance = DMA1_Stream7;/* Link hdma_tim to hdma[TIM_DMA_ID_CC3] (channel3) */
__HAL_LINKDMA(htim, hdma[TIM_DMA_ID_CC3], hdma_tim);DMA1->LIFCR = 0xFFFF;
DMA1->HIFCR = 0xFFFF;/* Initialize TIMx DMA handle */
HAL_DMA_Init(htim->hdma[TIM_DMA_ID_CC3]);}UPDATE: SOLVED
As JW pointed out, the memory address of the variable I was trying to transfer was in TCM memory, which DMA1 and DMA2 do not have access to. After adding __attribute__((section(''.sram_d2'')) to the definition of the variable, it was placed into SRAM in domain 2 (address 0x30000000), this solved the problem (YAY).
Solved! Go to Solution.
2018-04-09 12:08 PM
The DTCM-RAM is available only to the processor and MDMA. Use other RAM (preferrably one of those in the D2 domain).
JW
2018-04-09 12:08 PM
The DTCM-RAM is available only to the processor and MDMA. Use other RAM (preferrably one of those in the D2 domain).
JW
2018-04-09 7:38 PM
Take a look into this thread, at least for the ADC it helped with my problem: