cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32h743 gets hot on custom PCB

Bassam_Mostafa
Associate

I designed a PCB using the STM32H743 in the TFBGA240 +25 package.
When I power the board, the STM32 gets hot. I measured the voltage across the VCAP capacitors, and it is 2.2 V, while it should be a maximum of 1.35 V.
What could be causing the VCAP voltage to rise to 2.2 V?

2 REPLIES 2
TDK
Super User

Only a bad schematic design or a manufacturing error will cause this.

Show a large in-focus picture of your chip and your schematic if you can.

If you feel a post has answered your question, please click "Accept as Solution".
Andrew Neil
Super User

Welcome to the forum.

Please see How to write your question to maximize your chances to find a solution for best results.

In particular, as it's a custom PCB, you will need to post your schematic & layout.

Some good, clear photos would also help.

 

Have you checked your design against Application note AN4938, "Getting started with STM32H74xI/G and STM32H75xI/G MCU hardware development"

Also check https://www.st.com/en/microcontrollers-microprocessors/stm32h743-753/documentation.html 

 


@Bassam_Mostafa wrote:

When I power the board, the STM32 gets hot. 


How hot, exactly?

What current is it drawing.

Have you loaded any code at this point?

 

PS:

Is this the first time this design has been use, or has it worked OK previously?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.