2023-08-11 4:11 AM
Hi STM32-Community,
I'm using an STM32H743 with ADC3 in circular DMA mode. ADC has a clockfrequency of 48 MHz. I'm using 8 channels within this ADC3 and also configured the DMA with said channels each with a sampling time of 64.5 cyles. I'm using an async prescaler of 6.
Calculating the sampling rate for a single ADC Channel I get:
48 MHz
----------------- = 15,504 Hz ~ 15.5 kHz
(8 Channels* 6 (Prescaler) * 64.5)
I've put a variable within my DMA routine (which does nothing else) and everytime the DMA toggles this variable, I send out the time needed between each DMA interrupt. I consistenly receive 1169 ms with a DMA Size of 65528.
65528
--------------------------------- ~ 7.005 kHz.
(1.169)*8 (ADC-Channels)
Where is my error?
Here are the ADC Config:
/* ADC3 init function */ void MX_ADC3_Init(void) { /* USER CODE BEGIN ADC3_Init 0 */ /* USER CODE END ADC3_Init 0 */ ADC_ChannelConfTypeDef sConfig = {0}; /* USER CODE BEGIN ADC3_Init 1 */ /* USER CODE END ADC3_Init 1 */ /** Common config */ hadc3.Instance = ADC3; hadc3.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV6; hadc3.Init.Resolution = ADC_RESOLUTION_16B; hadc3.Init.ScanConvMode = ADC_SCAN_ENABLE; hadc3.Init.EOCSelection = ADC_EOC_SINGLE_CONV; hadc3.Init.LowPowerAutoWait = DISABLE; hadc3.Init.ContinuousConvMode = ENABLE; hadc3.Init.NbrOfConversion = 8; hadc3.Init.DiscontinuousConvMode = DISABLE; hadc3.Init.ExternalTrigConv = ADC_SOFTWARE_START; hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hadc3.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR; hadc3.Init.Overrun = ADC_OVR_DATA_PRESERVED; hadc3.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE; hadc3.Init.OversamplingMode = DISABLE; if (HAL_ADC_Init(&hadc3) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_5; sConfig.Rank = ADC_REGULAR_RANK_1; sConfig.SamplingTime = ADC_SAMPLETIME_64CYCLES_5; sConfig.SingleDiff = ADC_SINGLE_ENDED; sConfig.OffsetNumber = ADC_OFFSET_NONE; sConfig.Offset = 0; sConfig.OffsetSignedSaturation = DISABLE; if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_9; sConfig.Rank = ADC_REGULAR_RANK_2; if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_4; sConfig.Rank = ADC_REGULAR_RANK_3; if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_8; sConfig.Rank = ADC_REGULAR_RANK_4; if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_3; sConfig.Rank = ADC_REGULAR_RANK_5; if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_7; sConfig.Rank = ADC_REGULAR_RANK_6; if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_2; sConfig.Rank = ADC_REGULAR_RANK_7; if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_6; sConfig.Rank = ADC_REGULAR_RANK_8; if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN ADC3_Init 2 */ /* USER CODE END ADC3_Init 2 */ }
CubeMX ADC-Frequency:
I know I'm not 100% correct with my method measuring the sampling frequency, but being that far off left me wondering what I'm doing wrong.
Kind regards
Solved! Go to Solution.
2023-08-11 5:22 AM - edited 2023-08-11 5:30 AM
You're missing:
An x2 prescaler on the ADC clock.
Extra samples due to the conversion (would be 8.5 for 16-bit conversion).
2023-08-11 5:22 AM - edited 2023-08-11 5:30 AM
You're missing:
An x2 prescaler on the ADC clock.
Extra samples due to the conversion (would be 8.5 for 16-bit conversion).
2023-08-11 6:22 AM
Thank you so much!
Have a nice week end!
2024-01-14 10:24 PM
Query: Using STM32H743XI EVAL BOARD,
ERROR IN READING 2 ADC1 CHANNEL (PA0_C, PA1_C) IN DMA CIRCULAR MODE -
1ST CHANNEL GIVING ACCURATE COUNTS,
2ND CHANNEL SET AT 2V - ALWAYS SHOWING COUNTS SAME AS OF 1ST CHANNEL, WHERE POT IS CONNECTED?
ADC CLOCK, CONFIGS AND DMA SETTINGS AS FOLLOWS:
Tried example code also from STM32H7cubmx package (1.11.0), same result? anything missing from above configuration?
2024-01-15 5:54 AM
Please don't duplicate post, especially in unrelated threads.
https://community.st.com/t5/stm32-mcus-products/stm32-gpio-sink-source-currents/m-p/628313#M232513