2023-08-08 2:33 PM - edited 2023-08-08 2:36 PM
I have a project running on my Stm32H7. I imported my ethernetif/lwip settings from the Stm32CubeH7 H723 lwip + freertos http server example, but made some small changes. For the most part in the most basic sense, the driver works and my board at least gets a DHCP lease and responds to ping, but I am getting an assert:
"Assertion "pbuf_free: p->ref > 0" failed at line 753 in [......]/LwIP/src/core/pbuf.c"
I've read so many topics on the state of Ethernet in the Stm32H7. Because of the ST community manager locking threads where fixes are discussed, I honestly don't know the current state of the drivers, except I can guess that this is an issue having to do with pbufs getting clobbered. I've seen the large zip file from https://community.st.com/t5/embedded-software-mcus/bug-fixes-stm32h7-ethernet/td-p/281420, but I don't know how out of date this is or how many of these issues have truly been fixed now.
If the drivers in the CubeH7 drivers are working, what am I doing wrong? If they are not, when can we expect better fixes? The Stm32H7 has been out for 6+ years.
Thanks!
Attached are my files:
NOTE: In my code, D/ICACHE are enabled in main
Solved! Go to Solution.
2023-08-23 6:09 PM
Thanks @STOne-32 , I will follow up with them.
2023-10-12 6:39 AM
Do you have any solution? I have exactly the same problem with pbuf assert.
2023-11-02 8:41 AM
Any update ? I have the exact same problem.
2024-02-10 7:22 AM
hi, i am also facing similar problem. did you get the solution? could you help ?
Sankar
2024-02-10 8:56 AM
2024-02-12 10:25 AM
Hello @Sankar ,@dumarjo, @kotofey,
I can confirm that this issue is related mostly to buffer sizes exceeding their dedicated memory addresses and this addressees can change based on the H7 series and if it's a dual or single core MCU . i don't know you exact issues but you can try to look for the following common mistakes:
a detailed explanation on the setup of Ethernet and LWIP on STM32H7 can be found in this article .
BR