cancel
Showing results for 
Search instead for 
Did you mean: 

stm32H723 (nucleo) with SDMMC, FR_NOT_READY

Tbill.1
Associate II

I'm stock since a while now.

I use H723 nucleo board with a SD card socket, build for SPI, but I use it as SDMMC with 1bit wide.

this socket is ok with SD and SPI.

f_mount send FR_NOT_READY.

I have the same answer with or with out Sd card...

I use a logic analyser and I can see that the clock never stop after start

is anybody have a clue or a simple working project with H723 and SDMMC ?

1 ACCEPTED SOLUTION

Accepted Solutions
Tbill.1
Associate II

It's working now, I make a(classic) mistakes : sd detection !

View solution in original post

1 REPLY 1
Tbill.1
Associate II

It's working now, I make a(classic) mistakes : sd detection !