cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 Nucleo TrueStudio Ethernet webserver project

robertnoble9
Associate III
Posted on June 03, 2018 at 01:21

Hi,

I have bee trying to get a TrueStudio ethernet project working correctly with an STM32H7 Nucleo board with little success. I'm trying to get the simple example webserver working from the Cu

beMX examples 

but I'm struggling gettting all of the required files in the right place.

Does anyone have an existing, working example of a TrueStudio web server project for the stm32H7 nucleo board that doesn't use the FreeRTOS?

Thanks in advance

#webserver #stm32h7-ethernet #atollic-truestudio #truestudio #atollic
1 REPLY 1
Imen.D
ST Employee
Posted on June 26, 2018 at 12:16

Hello

Noble.Robert.002

TrueSTUDIO projects are not provided in the Cube firmware package for all demonstrations.

Please find here a useful document that canhelp you to migrate from IAR to TrueSTUDIO (Which is GNU compiler based):

http://info.atollic.com/hs-fs/hub/460400/file-2676247878-pdf/AppNotes/AN1405_MigrateEclipseGCCtoTS.pdf

Migrating from other Eclipse/GCC IDEs to Atollic® TrueSTUDIO®. Then, do not hesitate to ask for helpwhen you have problems.

Hope this helps you.

With Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen