cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32h7 Memory location for boot on the M7 core and the M4 core? Looking for a detailed explanation on boot or start up procedure for a dual core product.

rwareinc
Associate III
 
1 ACCEPTED SOLUTION

Accepted Solutions
Uwe Bonnes
Principal III

What are you missing in RM0399?

View solution in original post

3 REPLIES 3
Uwe Bonnes
Principal III

What are you missing in RM0399?

rwareinc
Associate III

Turns out RM0399 is what I was missing... had RM0433, this covers it. Thanks

Options define start addresses/modes

Notionally the dual-port flash is shared, lower half to M7 (0x08000000), upper half to M4 (0x08100000), and most the lower bandwidth peripherals living in the same domain as the M4, but accessible to both.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..