2021-09-11 8:52 AM
I am working on NUCLEO-h745ziq board.I am interface i2c to BMP280 sensor using DMA method.But I am unable to read chipID .Using the polling method Iable to get chipiD and also temperature but using DMA i am unable please help me.
s8 BME280_I2C_bus_read(u8 dev_addr, u8 reg_addr, u8 *reg_data, u8 cnt)
{
HAL_StatusTypeDef status = HAL_OK;
s32 iError = BME280_INIT_VALUE;
u8 array[I2C_BUFFER_LEN] = {BME280_INIT_VALUE};
u8 stringpos = BME280_INIT_VALUE;
array[BME280_INIT_VALUE] = reg_addr;
//while (HAL_I2C_IsDeviceReady(&hi2c4, (uint16_t)(dev_addr<<1), 3, 100) != HAL_OK) {}
status = HAL_I2C_Mem_Read_DMA(&hi2c4, // i2c handle
(uint8_t)(dev_addr<<1), // i2c address, left aligned
(uint8_t)reg_addr, // register address
I2C_MEMADD_SIZE_8BIT, // bme280 uses 8bit register addresses
(uint8_t*)(&array), // write returned data to this variable
cnt // how many bytes to expect returned
); // timeout
if (status != HAL_OK)
{
// The BME280 API calls for 0 return value as a success, and -1 returned as failure
iError = (-1);
}
while (HAL_I2C_GetState(&hi2c4) != HAL_I2C_STATE_READY)
{
}
for (stringpos = BME280_INIT_VALUE; stringpos < cnt; stringpos++) {
*(reg_data + stringpos) = array[stringpos];
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_DIRECT_SMPS_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 100;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
}
return (s8)iError;
}
void HAL_I2C_MspInit(I2C_HandleTypeDef* hi2c)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
if(hi2c->Instance==I2C4)
{
/* USER CODE BEGIN I2C4_MspInit 0 */
/* USER CODE END I2C4_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2C4;
PeriphClkInitStruct.I2c4ClockSelection = RCC_I2C4CLKSOURCE_D3PCLK1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
__HAL_RCC_GPIOF_CLK_ENABLE();
/**I2C4 GPIO Configuration
PF14 ------> I2C4_SCL
PF15 ------> I2C4_SDA
*/
GPIO_InitStruct.Pin = GPIO_PIN_14|GPIO_PIN_15;
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.Alternate = GPIO_AF4_I2C4;
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
/* Peripheral clock enable */
__HAL_RCC_I2C4_CLK_ENABLE();
/* I2C4 DMA Init */
/* I2C4_RX Init */
hdma_i2c4_rx.Instance = BDMA_Channel0;
hdma_i2c4_rx.Init.Request = BDMA_REQUEST_I2C4_RX;
hdma_i2c4_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_i2c4_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_i2c4_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_i2c4_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_i2c4_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_i2c4_rx.Init.Mode = DMA_NORMAL;
hdma_i2c4_rx.Init.Priority = DMA_PRIORITY_VERY_HIGH;
if (HAL_DMA_Init(&hdma_i2c4_rx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hi2c,hdmarx,hdma_i2c4_rx);
/* I2C4_TX Init */
hdma_i2c4_tx.Instance = BDMA_Channel1;
hdma_i2c4_tx.Init.Request = BDMA_REQUEST_I2C4_TX;
hdma_i2c4_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_i2c4_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_i2c4_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_i2c4_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_i2c4_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_i2c4_tx.Init.Mode = DMA_NORMAL;
hdma_i2c4_tx.Init.Priority = DMA_PRIORITY_MEDIUM;
if (HAL_DMA_Init(&hdma_i2c4_tx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hi2c,hdmatx,hdma_i2c4_tx);
/* I2C4 interrupt Init */
HAL_NVIC_SetPriority(I2C4_EV_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(I2C4_EV_IRQn);
HAL_NVIC_SetPriority(I2C4_ER_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(I2C4_ER_IRQn);
/* USER CODE BEGIN I2C4_MspInit 1 */
/* USER CODE END I2C4_MspInit 1 */
}
}
2021-09-11 12:03 PM
Are you sure using local/auto variables is advisable for DMA buffers?
Do you manage cache coherency?
2021-09-14 9:11 PM
I am assign the variablein SRAM and updated in flash files.And aslo manage the cache but still get it read the NULL value i am unable to understand why its get