cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 FMC Interface to External Memory. Running code from external memory.

KGane.1
Associate III

Hi,

I am considering upgrade from STM32F4 series to STM32F7 or STM32H7(single core) series. However, the H7 embedded memory is not enough for the requirement. I would like to run simple RTOS scheduler. So there is need for external memory.

-QuadSPI interface - Flash(code and config storage)

I would like to interface the following through FMC

-PSRAM(program memory)

-SRAM(data memory)

-FPGA(memory mapped)

I have two questions.

  1. What are the drawbacks of running code from external memory
  2. Is it possible to interface(PSRAM,SRAM and FPGA to FMC)

Thanks

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
TDK
Super User

> What are the drawbacks of running code from external memory

It will be slower, and it's more complicated to load code onto external memory than the internal flash.

> Is it possible to interface(PSRAM,SRAM and FPGA to FMC)

PSRAM/SRAM yes. An FPGA can appear as anything, so yes, assuming you have compatible code on it. I would recommend doing a pinout in CubeMX to verify all pins are available.

If you feel a post has answered your question, please click "Accept as Solution".

Some reason you'd use SRAM/PSRAM over a large SDRAM?

You can have up to 256 MB of QuadSPI Flash allowing for execute-in-place. Can be banked to provide 8-bit.

eMMC on the SDMMC could provide for very large storage of data/code.

Watch out for having enough select pins, although you could divide down and decode a larger one externally.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
KGane.1
Associate III

@TDK​ Thanks. Agree. There would be lot of work in bootloader to load code from external flash to external RAM.

Reference manual says..."The FMC outputs a unique Chip Select signal, NE[4:1], per bank. All the other signals (addresses, data and control) are shared."

So using chip select, we can map

-PSRAM to FMC-NOR Flash/PSRAM Controller NE[1]

-SRAM to FMC-NOR Flash/PSRAM Controller NE[2]

-FPGA to FMC-NOR Flash/PSRAM Controller NE[3]

or

-PSRAM to FMC-NOR Flash/PSRAM Controller NE[1]

-SRAM to FMC-NOR Flash/PSRAM Controller NE[2]

-FPGA to FMC SDRAM Controller

@Community member​ Thanks. Seems i have to read application note about QuadSPI Flash XIP. Would it affect performance comparing to parallel interface?

Caching should mask the inherent/relative slowness of the SDRAM, or QSPI external memories.

Code could always be copied into a RAM.

In indirect mode the QSPI can address 4GB devices.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..