2021-03-05 6:47 AM
Using STM32H743ZI
I am using SPI1 in 2 lines Rx only mode with DMA2 Stream 2 as in ST example
I use Rx DMA with a buffer located in D2 RAM. Using debugger I found that the first reception works well, data gets written into my buffer. But my DMA doesn't fire any interrupt, so the next transfers do not work.
Here is my init code :
hdma_spi1_rx.Instance = DMA2_Stream2;
hdma_spi1_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
hdma_spi1_rx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_spi1_rx.Init.MemBurst = DMA_MBURST_INC4;
hdma_spi1_rx.Init.PeriphBurst = DMA_PBURST_INC4;
hdma_spi1_rx.Init.Request = DMA_REQUEST_SPI1_RX;
hdma_spi1_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_spi1_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi1_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi1_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi1_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi1_rx.Init.Mode = DMA_NORMAL;
hdma_spi1_rx.Init.Priority = DMA_PRIORITY_HIGH;
if (HAL_DMA_Init(&hdma_spi1_rx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hspi,hdmarx,hdma_spi1_rx);
/* SPI1 interrupt Init */
__HAL_SPI_ENABLE_IT(hspi, SPI_IT_RXNE) ;
/* USER CODE BEGIN SPI1_MspInit 1 */
HAL_NVIC_SetPriority(DMA2_Stream2_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream2_IRQn);
HAL_NVIC_SetPriority(SPI1_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(SPI1_IRQn);
Any idea why my DMA2 peripheral wont trigger interrupt ?
Solved! Go to Solution.
2021-03-08 6:47 AM
My interrupts are working now, I added some flag clearing bare metal programming and removed breakpoints and it works now thanks !
2021-03-05 6:53 AM
Do other interrupts work?
Using .cpp or C++ ?
The linker binds your IRQHandler?
2021-03-05 6:55 AM
I2C4 interrupts works. I am using .c, I am using GNU C
How can i check if my linker binds my IRQHandler ? in .map ?
2021-03-05 7:09 AM
> How can i check if my linker binds my IRQHandler ? in .map ?
The best way is to look at disasm and check if the ISR's address (e.g. as found in mapfile) is at the required position of the vector table (see startup file for the vector tables' source).
Some general hints to debug interrupts here.
JW
2021-03-05 7:30 AM
I checked DMA2 status register with debugger, after the first Rx. Both Half transfert complete flag and Transfert complete flag are 1.
It means my peripheral is working well. Do you have some link I can look to learn how to check the vector table ? I have never done it
2021-03-05 8:40 AM
Update I also checked NVIC ISER and NVIC->ISER[1]=0x400 0000 which means the bit 58 is 1, it is DMA2 Stream2 interrupt
2021-03-05 6:42 PM
Is a function DMA2_Stream2_IRQHandler implemented somewhere? This is your handler.
This name must be exactly same as defined in your startup_stm32h743xx.s
--pa
2021-03-05 8:05 PM
How do you know the interrupt doesn't fire?
Are the HT and TC interrupts enabled locally, i.e. in respective DMA stream's control register?
You get the ISR address from mapfile or disasm view of that function in IDE, and then dump content of vector table e.g. in memory view of IDE.
Also, IMO, having an SPI interrupt together with DMA is nonsense, although it probably does not cause you the immediate problem.
JW
2021-03-08 12:35 AM
@Pavel A.
In my startup_stm32h743xx.s, DMA2_Stream2_IRQHandler is registered here :
And in "stm32h7xx_it.c" :
void DMA2_Stream2_IRQHandler(void)
{
HAL_DMA_IRQHandler(&hdma_spi1_rx);
}
@Community member
I know the interrupt doesnt fire because I put a breakpoint in DMA2_Stream2_IRQHandler()
Also, you think I shouldn't enable SPI1 interrupts ? Does the SPI throw an End of Tranfert interrupt when DMA is done or when it starts transfering ?
From looking at map file, DMA2_Stream2_IRQHandler address is 0x0000000008000fa0
With memory browser, I see a 08000FA1 value at 0x8000128 address.
It is the correct position and value (good news but bad news for diagnostic)
Also I checked and SCB->VTOR = 0x8000000
2021-03-08 2:40 AM
Gabriel,
All you wrote above looks OK.
You've already checked that the HT and TC flags are set in the DMA status register, but are the HT and TC interrupts enabled locally, i.e. in respective DMA stream's control register?
The SPI interrupt: I don't use the 'H7 and I know its SPI is a very complicated beast, so there may be some merit in using it. I am not going to investigate this further, nor am I going to investigate what the Cube/HAL incantations you've used are supposed to do. In the older/simpler STM32, it's the DMA which is supposed to clear the SPI's RXNE status bit by reading the data.
JW